1.1.2.4.2 DRV_AK4954_Close Function
void DRV_AK4954_Close( DRV_Handle handle )Summary
Closes an opened-instance of the AK4954 driver
Description
This routine closes an opened-instance of the AK4954 driver, invalidating the handle. Any buffers in the driver queue that were submitted by this client will be removed. After calling this routine, the handle passed in "handle" must not be used with any of the remaining driver routines. A new handle must be obtained by calling DRV_AK4954_Open before the caller may use the driver again.
Preconditions
The DRV_AK4954_Initialize routine must have been called for the specified AK4954 driver instance.
DRV_AK4954_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
Usually there is no need for the driver client to verify that the Close operation has completed. The driver will abort any ongoing operations when this routine is called.
Example
DRV_HANDLE handle; _\/\/ Returned from DRV_AK4954_Open_ DRV_AK4954_Close(handle);
C
void DRV_AK4954_Close(const DRV_HANDLE handle);