1.1.3.4.1 DRV_GENERICCODEC_Open Function
DRV_HANDLE DRV_GENERICCODEC_Open ( const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT ioIntent )
Summary
Opens the specified Generic Codec driver instance and returns a handle to it
Description
This routine opens the specified Generic Codec driver instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the driver. The ioIntent parameter defines how the client interacts with this driver instance.
The DRV_IO_INTENT_BLOCKING and DRV_IO_INTENT_NONBLOCKING ioIntent options are not relevant to this driver. All the data transfer functions of this driver are non blocking.
Generic Codec can be opened with DRV_IO_INTENT_WRITE, or DRV_IO_INTENT_READ or DRV_IO_INTENT_WRITEREAD
io_intent option. This decides whether the driver is used for headphone output, or microphone input or both modes simultaneously.
Specifying a DRV_IO_INTENT_EXCLUSIVE will cause the driver to provide exclusive access to this client. The driver cannot be opened by any other client.
Preconditions
Function DRV_GENERICCODEC_Initialize must have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| drvIndex | Identifier for the object instance to be opened |
| ioIntent | Zero or more of the values from the enumeration DRV_IO_INTENT "ORed" together to indicate the intended use of the driver. See function description for details. |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).
If an error occurs, the return value is DRV_HANDLE_INVALID. Error can occur
- if the number of client objects allocated via DRV_GENERICCODEC_CLIENTS_NUMBER is insufficient.
- if the client is trying to open the driver but driver has been opened exclusively by another client.
- if the driver hardware instance being opened is not initialized or is invalid.
- if the ioIntent options passed are not relevant to this driver.
Remarks
The handle returned is valid until the DRV_GENERICCODEC_Close routine is called. This routine will NEVER block waiting for hardware.If the requested intent flags are not supported, the routine will return DRV_HANDLE_INVALID. This function is thread safe in a RTOS application. It should not be called in an ISR.
Example
DRV_HANDLE handle;
handle = DRV_GENERICCODEC_Open(DRV_GENERICCODEC_INDEX_0, DRV_IO_INTENT_WRITEREAD | DRV_IO_INTENT_EXCLUSIVE); if (DRV_HANDLE_INVALID == handle) {
_// Unable to open the driver_ _// May be the driver is not initialized or the initialization_ _// is not complete._
}C
DRV_HANDLE DRV_GENERICCODEC_Open(const SYS_MODULE_INDEX iDriver, const DRV_IO_INTENT ioIntent);