1.1.1.4.4 DRV_AK4953_MicMuteOff Function
void DRV_AK4953_MicMuteOff(DRV_HANDLE handle)Summary
Umutes th AK4953's microphone input.
Description
This function unmutes the AK4953's microphone input.
Preconditions
The DRV_AK4953_Initialize routine must have been called for the specified AK4953 driver instance.
DRV_AK4953_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
_\/\/ myAppObj is an application specific object._ MY_APP_OBJ myAppObj; _\/\/ myAK4953Handle is the handle returned \/\/ by the DRV_AK4953_Open function._ DRV_AK4953_MicMuteOff(myAK4953Handle); _\/\/AK4953 microphone unmuted_
C
void DRV_AK4953_MicMuteOff(DRV_HANDLE handle);