1.1.5.2.2 DRV_I2S_Close Function
void DRV_I2S_Close( DRV_Handle handle )Summary
Closes an opened-instance of the I2S driver.
Description
This routine closes an opened-instance of the I2S driver, invalidating the handle. Any buffers in the driver queue that were submitted by this client will be removed. A new handle must be obtained by calling DRV_I2S_Open before the caller may use the driver again.
Preconditions
DRV_I2S_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
_// 'handle', returned from the DRV_I2S_Open_ DRV_I2S_Close(handle);
C
void DRV_I2S_Close(const DRV_HANDLE handle);