4.6 Get Device Support for MPLAB® X
MPLAB X: Use the MPLAB Pack Manager, found under Tools → Packs, to add support for new devices in MPLAB X.
For the AVR® EA Family, update to the latest version by
performing the following steps:
- Click Check for Updates.
- For the AVR® EA Family, select the latest available version of AVR-Ex_DFP.
- Click Install.
For offline installers, go to packs.download.microchip.com/. Double click on the installer file and follow the instructions to install a package. Any open MPLAB X window must be closed for the installation to take effect.