4 Installing the Library
To install the MCC Melody 8-Bit MDFU Client Library:
Content Manager Wizard
- Create a new MPLAB® X project with one of the supported Melody devices.
- Open MCC.
- Select MCC Melody from the Content Manager Wizard start page.
- Once you see the MCC Content Manager Wizard page with required and optional content boxes, check the box located next to the 8-Bit MDFU Client library. It can be found on this page by going to Optional Content > Libraries > Bootloader.
- Once the box there is checked, click Finish to start the library download.
Content Manager
- Open MCC.
- Select Content Manager from within the Device Resources section.
- Navigate to Libraries > Bootloader > 8-Bit MDFU Client and select the desired version.
- Click Apply in the top right of the Content Manager Window.
For a detailed guide on installation, refer to the Getting Started Guide.