2.1 Basic Concept
Note that this section is not meant to be a comprehensive analysis of the theory of operation, rather a quick description to offer a more intuitive sense of how a DAB works.
The DAB converter works on the principle of AC power transfer. In essence, one AC voltage source/load is connected to another AC voltage source/load through an inductor. See Figure 2-1. V1 and V2 are AC sources with a frequency (ω) and a phase difference θ (V1 is taken as the reference). The power transfer between V1 and V2 can be controlled by the phase shift, θ.
What equation governs the power transfer from V1 to V2 or visa-versa? First, determine the inductor current IL(t) and then determine the average power. The instantaneous inductor current IL(t) is defined in Equation 2-1.
Assuming a power flow from left to right, the instantaneous power flowing from V1 to V2 is defined in Equation 2-2.
The average power PAVG over an AC period 1/ω is defined in Equation 2-3.
Working through the mathematics, the average power transfer is defined in Equation 2-4.
Equation 2-4 is very important. It says that depending on θ, the power transferred between the two AC sources can be modulated. The magnitude of the power can also be controlled by controlling the magnitudes of the AC waveforms (namely V1 and V2) and the frequency of the AC waveforms ω.