2.6 EntityName Object
The EntityName object is used to identify an entity responsible for a specific aspect of the secure sub-system device. The members in this object are variable and must be the same as the attributes defined in section 6 of ITU-T X.520 (ISO/IEC 9594-6). While none of the members are required, at least one must be present. The example below shows typical use with Organization Name (6.4.1) and Organizational Unit Name (6.4.2).
{
"organizationName": "Microchip Technology Inc",
"organizationalUnitName": "Secure Computing Group",
}| organizationName | Name of the entity organization (e.g., company name). |
| organizationalUnitName | Optional name of a unit within the organization to which the entity pertains. |