8.3 Sequential Read within the EEPROM
Sequential reads start as either a current address read or as a random
read. However, instead of the host sending a NACK (logic ‘1’) response to
end a read operation after a single byte of data has been read, the host sends an ACK
(logic ‘0’) to instruct the AT21CS01/AT21CS11 to
output another byte of data. As long as the device receives an ACK from the host after each
byte of data has been output, it will continue to increment the address counter and output
the next byte of data from the EEPROM. If the end of the EEPROM is reached, then the
Address Pointer will “roll over” to the beginning (address 00h) of the EEPROM region. To
end the sequential read operation, the host must send a NACK response after the device has
output a complete byte of data. After the device receives the NACK, it will end the read
operation and return to Standby mode.