8.1 Current Address Read within the EEPROM
The internal Address Pointer must be pointing to a memory location within
the EEPROM in order to perform a current address read from the EEPROM. To initiate the
operation, the host must send a Start condition, followed by the device address byte with
the opcode of 1010b (Ah) specified, along with the appropriate client
address combination and the Read/Write bit set to a logic
‘1’. After the device address byte has been sent, the AT21CS01/AT21CS11 will return an ACK (logic ‘0’).
Following the ACK, the device is ready to output one byte (eight bits) of
data. The host initiates all bits of data by driving the SI/O line low to start. The AT21CS01/AT21CS11 will hold the line low after the host releases it to
indicate a logic ‘0’. If the data is logic ‘1’, the AT21CS01/AT21CS11 will not hold the SI/O line low at all, causing it to
be pulled high by the pull-up resistor once the host releases it. This sequence repeats for
eight bits.
After the host has read the first data byte and no further data is
desired, the host must return a NACK (logic ‘1’) response to end the read
operation and return the device to the Standby mode. Figure 8-1 depicts this sequence.
If the host would like the subsequent byte, it would return an ACK (logic
‘0’) and the device will be ready to output the next byte in the memory
array. Refer to Sequential Read within the EEPROM for details about continuing to read beyond
one byte.