9.8.3 Updating the Accelerator Firmware from Accelerator Level

Use the Firmware Update wizard to update the firmware for one or more accelerator of the same type on the local or a remote system.

To update the accelerator firmware:
  1. In Enterprise View, select a system.
  2. On the ribbon, in the System group, click Firmware Update.

    The Firmware Update window opens.

  3. In the Select Files panel, click Choose to browse the file for the firmware update (typically, a .bin file). Click Open to select the file (the button label may be different on your browser).

    The file name appears in the Uploaded Firmware File(s) list.

  4. Click Next to review the summary, then click Finish.
    CAUTION: Do not power down the server while the update is in progress.
  5. When the update completes, click OK. Restarting the server may require activating the new firmware image.