10.2.1 Locating Physical Drives

To locate an individual physical drive or all physical drives on the controller:

  1. In the Enterprise View, select a controller or an individual drive on the controller.
  2. On the ribbon, in the Physical Device group, click Locate Physical Device.
    The Locate Physical Device window opens.
  3. From the drop-down list, select the timeout period (1 hour, 4 hours, 24 hours).
  4. Click the Locate button.
    The LED on the physical drive(s) begin to blink.
  5. To stop blinking the drive(s) immediately, click Stop.
  6. Click Cancel to close the Locate Physical Device window.
    The LED(s) continue to blink for the duration of the timeout period.