8.2.1 Disabling SED Based Encryption

Perform the following steps to disable the SED based encryption:
  1. Open the Self Encrypting Drive (SED) Based Encryption dialog box and then click the Settings tab.
  2. Select the Disable SED Based Encryption check box and then click OK.

    This removes the SED based encryption configuration.

Graphical user interface, application Description automatically generated

Disable SED Based Encryption check box is disabled if one or more SED is not in Original Factory State (OFS) or SED Encryption has Waiting on Controller Password status.