10.8.2 Updating the Accelerator Firmware
Use the Firmware Update wizard to update the firmware for one or more accelerator of the same type on the local or a remote system.
To update the accelerator firmware:
- In Enterprise View, select a system.
- On the ribbon, in the System group, click Firmware Update.

The Firmware Update window opens.
- Select Accelerator from the Select Device Type panel, then click
Next.

- Select the accelerators that need to be updated the Select Devices panel, then
click Next.

- In the Select Files panel, click Choose to browse the file for the firmware
update (typically, a .bin file). Click Open to select the file (the
button label may be different on your browser).

The file name appears in the Uploaded Firmware File(s) list.
- Click Next to review the summary, then click Finish.
CAUTION: Do not power down the server while the update is in progress. - When the update completes, click OK. Restarting the server may require activating the new firmware image.