6.3 Assigning a Dedicated Hot Spare
A dedicated hot spare is assigned to one or more arrays. It will protect any redundant logical drive on those arrays.
Note: You must create
the array before you can assign a dedicated hot spare to protect
it.
To assign a dedicated spare:
- In the Enterprise View, select a controller, an array on that controller, or a Ready physical drive.
-
On the ribbon, in the Physical Device group, click
Spare Management.The Spare Management wizard opens.
-
Select the Dedicated spare type, then
click Next.
-
If you selected a physical drive in the Enterprise view, select
the arrays you want to protect with a dedicated spare, then click
Next.
-
If you selected an array in the Enterprise view, select the
physical drive(s) you want to dedicate as hot spares, then click
Next. For details on SED support operations,
see Spare Management. (See Hot Spare Limitations for help selecting drives.)
- Review the summary of dedicated spares and protected arrays, then click Finish.