5.5.2 Moving a Logical Drive
A 4K SAS or 4K SATA logical device can be moved to another array of 4K SAS or 4K SATA drives, but cannot be moved to an array with 512-byte drives.

-
Moving to a new array: all SATA and SAS 4K drives that are
available to move to a new array are listed.

-
Moving to an existing array: if the logical device has already been created in a
different array using 4K drives, then the option will move a logical device to the
existing array of the same block size SAS/SATA 4K drives. Only arrays created using 4K
drives will be listed (512-byte arrays will not be listed).