5.5.3 Modifying a Logical Drive
Arrays created using 4K drives can be modified.

-
Moving drive(s): Moving a drive from one array to another array using the same
interface type. For example, if an array is created using 4K SATA drives, then you can
move a drive(s) from that array to a separate array that also uses 4K SATA drives.

-
Changing drive types: Changing the drive interface type from SAS to SATA or from SATA
to SAS. For example, if an array is created using 4K SAS drives, you can change the drive
type to 4K SATA drives only.