5.5.5 Assigning Spares at the Physical Device Level
Spares for 4K logical drives can be assigned at the physical device level.

If array/logical device is created with 4K SAS drives, then only
logical devices that were created with 4K SAS drives are listed.

Note:
maxCache cannot be created using 4K SATA drives.
512-byte maxCache cannot be assigned to 4K logical devices.
Drive interface types and drive block sizes cannot be mixed.
For example, SATA drives and SAS drives of the same block size cannot be mixed; 512-byte drives and 4K drives of the same interface type cannot be mixed.