Power ON the PolarFire Evaluation
board by sliding the SW3 switch.
On the host PC, launch the GUI.
Before connecting to the PolarFire Evaluation board, the GUI shows the default
values of the image size as 6183952 Bytes and target version number fields as
0. The GUI title also remains in grey colour, as shown in
the following figure.Figure 6-1. GUI Before
Connection
The GUI automatically detects the COM port and establishes a serial
connection. After the PolarFire Evaluation board is connected, the GUI
confirms the connection changing the GUI title to blue color. Also, the
Target Version is updated with the actual target
version number. The default image size is 6183952 Bytes. After connecting,
the GUI switches to the IAP mode as shown in the following figure.Figure 6-2. GUI After
Connection
Select the Image
Transfer option and click Initiate to
start the transfer of the IAP image to the SPI Flash of IAP Target. The image
transfer status is displayed as shown in the following figures.Figure 6-3. Image Transfer
ProgressFigure 6-4. Image Transfer
Complete
Select Authentication
IAP Image and click Initiate to start the
authentication of the IAP image by IAP Target.
When Authentication
IAP Image is selected, IAP Initiator sends appropriate
commands to initiate the authentication process at IAP Target’s end. The
authentication status is displayed as shown in the following figures.Figure 6-5. Authenticating IAP
ImageFigure 6-6. Authentication
Successful
Note: Authentication can be selected only after
the completion of Image Transfer showing a green tick.
Select the Program the
Image option and click Initiate. IAP
Initiator sends the appropriate command to IAP Target device to initiate the IAP
sequence. The programming progress is displayed as shown in the following
figure.Figure 6-7. Programming
Status
Note: The Program the Image
command can only be selected along with Authenticate IAP
Image command.
The execution time and updated target version are displayed as status, see
the following figure.Figure 6-8. Programming
Successful
To run all the three IAP commands in sequence, enable the Select
All check box and click initiate.
This concludes executing IAP. See the next section to execute data loopback.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.