5.1 SAMA5D29
| No. | Title/Link |
Hardware Board/ Kit Used | Description |
|---|---|---|---|
| 1 | Developing Applications with MPLAB Harmony v3 Software Framework for MPUs | NA | Step-by-step guide explaining:
|
| 2 | SAMA5D2 Series Boot Process Training Module | SAMA5D2 Series | The boot process of the SAMA5D2 series microprocessors (MPU) |
| 3 | MPLAB Discover Code Examples | SAMA5D2 Series | MPLAB Discover code examples |
| 4 | MPLAB github Examples | SAMA5D2 Series | MPLAB Harmony v3 application examples (CSP, Graphics, Ethernet, etc.) |
| 5 | SAMA5D29-Curiosity Development Board Introduction | SAMA5D29-Curiosity | Introduction to the SAMA5D29-Curiosity board |
| 6 | SAMA5D29-Curiosity – Features | SAMA5D29-Curiosity | Features of the SAMA5D29 Curiosity Board (EV07R15A) |
| 7 | Starting Linux OS Development on SAMA5D29-Curiosity | SAMA5D29-Curiosity | Step-by-step guide on how to get started developing a Linux OS application on the SAMA5D29-Curiosity development board |
| 8 | Booting a Demo Linux Image from an SD Card | SAMA5D29-Curiosity | Step-by-step instructions for booting a demonstration Linux image written to a microSD card on the SAMA5D29-Curiosity development board |
| 9 | Configure and Build at91bootstrap for an MPLAB Harmony v3 Project with MPLAB X IDE | SAMA5D29-Curiosity | How to configure and build at91bootstrap to debug an MPLAB Harmony v3 project with MPLAB X IDE on the SAMA5D29-Curiosity development board |
| 10 | Console Serial Communications | SAMA5D29-Curiosity | How to connect a host computer running a terminal emulation program to the SAMA5D29-Curiosity serial debug port (J28) to access the console |
| 11 | Getting Started with MPLAB Harmony v3 Development | SAMA5D29-Curiosity | A detailed guide on getting started with MPLAB Harmony v3 application development with a sample CSP application: PIO LED ON/OFF interrupt |
| 12 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SQI™ Flash Memory | SAMA5D29-Curiosity | How to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an SQI™ Flash memory |
| 13 | Writing MPLAB Harmony v3 Application and at91bootstrap to SQI Flash Memory Using SAM-BA ISP | SAMA5D29-Curiosity | How to write an MPLAB Harmony v3 application and at91bootstrap to an SQI Flash memory using SAM-BA® ISP |
| 14 | Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SD Memory Card | SAMA5D29-Curiosity | How to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an SD memory card |
| 15 | Copy MPLAB Harmony v3 Application and at91bootstrap to SD Memory Card | SAMA5D29-Curiosity | How to copy an MPLAB Harmony v3 application and at91bootstrap to an SD memory card |
| 16 | Read and Write Boot Configuration Word Using SAM-BA In System Programmer (ISP) | SAMA5D29-Curiosity | How to read and write the Boot Configuration Word from the Secure Fuse Controller (SFC) and Backup registers (BUREGn) using the SAM-BA In System Programmer (ISP) |
| 17 | Getting Started with the SAMA5D29-Curiosity Board (EV07R15A) Technical Brief | SAMA5D29-Curiosity | How to configure the boot sequence to boot from the user-preferred Non-Volatile Memory (NVM) using SAM-BA commands for the SAMA5D29-Curiosity board (EV07R15A) |
| 18 | CANFD and LCD integration MPLAB Harmony Demo Application | SAMA5D29-Curiosity | Demo application showing how to integrate CAN FD and LCD on the SAMA5D29-Curiosity board |
| 19 | SAM-BA In-System Programmer (ISP) | N/A | Introduction to SAM-BA ISP and command line interface |