1 External Interrupt – Overview

Interrupts are signals provided to the CPU of the microcontroller unit, either from internal peripheral modules or from external pins of the MCU. It alters the regular flow of the program execution by enabling the CPU to make a jump to execute instruction routines in some pre-defined location based on the interrupt that occurred. When the CPU completes the routine, it gets back to the location from where it had made a jump.

These pre-defined locations are called as the interrupt vector addresses or interrupt vectors.

An interrupt causes the device to save its state of execution and start executing the interrupt handler. For Atmel AVR Microcontrollers the PC register is the only register that will be saved and the stack pointer register is updated in the event of an interrupt. It is up to the user to save other registers like the status register, 32 general purpose registers (register file), on an event of an interrupt, if there is such a requirement in the application.

The interrupts are commonly used to save more time (such as multitasking) than the conventional polling method (waiting for the event to occur indefinitely).