33.4 Computation Operation

The ADC module hardware is equipped with post-conversion computation features. These features provide post-processing functions such as digital filtering/averaging and threshold comparison. Based on computation results, the module can be configured to take additional samples or stop conversions and an interrupt may be asserted.

Figure 33-11. Computational Features Simplified Block Diagram
The operation of the ADC computational features is controlled by the MD bits.

The module can be operated in one of five modes:

  • Basic: This is a Legacy mode. In this mode, ADC conversion occurs on single (DSEN = 0) or double (DSEN = 1) samples. ADIF is set after each conversion is complete. ADTIF is set according to the Calculation mode.
  • Accumulate: With each trigger, the ADC conversion result is added to the accumulator and ADCNT increments. ADIF is set after each conversion. ADTIF is set according to the Calculation mode.
  • Average: With each trigger, the ADC conversion result is added to the accumulator. When the RPT number of samples have been accumulated, a threshold test is performed. Upon the next trigger, the accumulator is cleared. For the subsequent tests, additional RPT samples are required to be accumulated.
  • Burst Average: At the trigger, the accumulator is cleared. The ADC conversion results are then collected repetitively until RPT samples are accumulated and finally the threshold is tested.
  • Low-Pass Filter (LPF): With each trigger, the ADC conversion result is sent through a filter. When RPT samples have occurred, a threshold test is performed. Every trigger after that, the ADC conversion result is sent through the filter and another threshold test is performed.

The five modes are summarized in the following table.

Table 33-2. Computation Modes
Mode MD Register Clear Event Value after Cycle(1) Completion Threshold Operations Value at ADTIF Interrupt
ADACC and CNT ADACC ADCNT Retrigger Threshold Test Interrupt AOV ADFLTR ADCNT
Basic 0 ACLR = 1 Unchanged Unchanged No Every Sample If threshold=true N/A N/A count
Accumulate 1 ACLR = 1 S1 + ADACC or (S2-S1)(2) + ADACC If (ADCNT = 0xFF): ADCNT, otherwise: ADCNT+1 No Every Sample If threshold=true ADACC Overflow ADACC/2CRS count
Average 2 ACLR = 1 or ADCNT ≥ ADRPT at GO set or retrigger S1 + ADACC or (S2-S1) + ADACC If (ADCNT = 0xFF): ADCNT, otherwise: ADCNT+1 No If ADCNT ≥ ADRPT If threshold=true ADACC Overflow ADACC/2CRS count
Burst Average 3 ACLR = 1 or at GO set or retrigger Each repetition: same as Average End with sum of all samples Each repetition: same as Average End with ADCNT = ADRPT Repeat while ADCNT < ADRPT If ADCNT ≥ ADRPT If threshold=true ADACC Overflow ADACC/2CRS ADRPT
Low-pass Filter 4 ACLR = 1 S1 + ADACC-ADACC/
2CRS or (S2-S1) + ADACC-ADACC/2CRS If (ADCNT = 0xFF): ADCNT, otherwise: ADCNT+1 No If ADCNT ≥ ADRPT If threshold=true ADACC Overflow ADACC/2CRS (Filtered Value) count
Note:
  1. When DSEN = 0, Cycle means one conversion. When DSEN = 1, Cycle means two conversions.
  2. S1 and S2 are abbreviations for Sample 1 and Sample 2, respectively. When DSEN = 0, S1 = ADRES; when DSEN = 1, S1 = ADPREV and S2 = ADRES.