1.2.4 EtherCAT Counter-Trigger and FoE Application for EVM_LAN9255_SAME53 SPI Communication
This EtherCAT example application demonstrates Counter-Trigger and Firmware Update over EtherCAT capability with SPI communication. The Counter and Trigger parameters are configured in the < ethercat repo >/apps/ethercat_counter_foe_app/firmware/src/slave_stack/lan9255 and demonstrates the communication between the EtherCAT Manager (TwinCAT Manager) and the EtherCAT Client (EtherCAT LAN9255).The firmware update is performed by FoE (File over EtherCAT) protocol. It is triggered by the EtherCAT Manager (TwinCAT Manager) which then download the firmware onto the EtherCAT Client (EtherCAT LAN9255) communication with EVB_LAN9255_SAME53 board.
This demonstration help document contains the following sections:
- MPLAB® Harmony Software Setup
- Hardware Setup
- Beckhoff Client Stack Code (SSC) Generation
- MPLAB® Harmony Code & Project Configuration
- Completing The EtherCAT Application
- Running The Application
- TwinCAT Manager and Microchip EtherCAT Client communication
- EtherCAT interface detect and EEPROM Programming
- Trigger and Counter Demonstration
- File over EtherCAT communication
- TwinCAT Manager and Microchip EtherCAT Client communication
MPLAB® Harmony Software Setup
The following MPLAB® software components are a prerequisite for the rest of the steps in this demonstration. Please follow the download and installation instructions available at below links.
- MPLAB® X Integrated Development Environment
- MPLAB® XC32/32++ C Compiler
- MPLAB® Harmony Configurator
- On the management PC, download and Install on the TwinCAT 3 Engineering Full Setup at https://www.beckhoff.com/english.asp?download/tc3-download-xae.htm. Select the latest TwinCAT 3.1 Version and click on the link. Note the dialog box shows the TwinCAT tool that will be installed TC31-Full-Setup.3.1.XXXX.XX and click on “Start Download”. Follow instructions to download.
Hardware Setup
The following tools will be used to program and debug the application on the target hardware.
- MPLAB® ICD4 + ICD4/PICKIT 3 Target Adapter Board using JTAG interface.
The following development board will be used for EtherCAT application development and run the application.
- LAN9255 - EtherCAT Client Controller
evaluation kit with SAME53 Microcontroller
The instructions in this guide are also applicable to other development boards with LAN9255 EtherCAT Client device. Hardware settings are board dependent and may vary between boards.
- Connect a micro USB cable to J8 port for power source.
- For programming, Connect a ICD4 JTAG cable to the J10 port of the EVB_LAN9255_SAME53 board.
- Connect RJ45 connector J1 to the TwinCAT Manager.
- Jumper setup for LAN9255 device w.r.t to different mode
- Block diagram of the EVB_LAN9255_SAME53 board
Beckhoff Client Stack Code (SSC) Generation
Follow instruction at this link to generate Beckhoff Client Stack Code: Steps to generate Beckhoff Client Stack Code.
MPLAB® Harmony Project Configuration
The present MPLAB Harmony v3 project is based on both MPLAB Code Configurator (MCC) and MPLAB Harmony3 Project Configurator (MHC).
To work with MCC, user require to follow the steps that is mentioned in the below link
https://microchipdeveloper.com/harmony3:update-and-configure-existing-mhc-proj-to-mcc-proj
microchipdeveloper.com/harmony3:getting-started-training-module-using-mcc
There are two options available for downloading/installing the MPLAB® Harmony Software Repositories from github & gitee.
The required repositories can be cloned from the github (or gitee) by using a local git client (such git bash). The MPLAB® Harmony Repositories are available at the following links:
https://github.com/Microchip-MPLAB-Harmony/
https://gitee.com/Microchip-MPLAB-Harmony/
The csp, dev_packs, mcc (or mhc) and ethercat repositories should be cloned. The required repositories can also be cloned (downloaded) or previously downloaded repositories can be updated by using the MPLAB® Harmony 3 Content Manager. The following sections provide details on using the MPLAB® Harmony 3 Content Manager to download the repositories.
- Refer to the EtherCAT MPLAB® Harmony Software Setup https://github.com/Microchip-MPLAB-Harmony/ethercat/wiki/create-your-first-ethercat-application details to create a EtherCAT project.
- The following Project Graph diagram shows the required Harmony components those are included for the present EtherCAT application for the EVB_LAN9255_SAME53 board.
- Click on the EtherCAT Stack in the Project Graph window. In the Configuration
window,
- The Beckhoff Client Stack source directory path should point to the folder that contains the files generated by the SSC tool.
- Enable FoE checkbox enables File over EtherCAT feature.
- Click on LAN9255 component from the project graph.
- EtherCAT Interrupt Priority Level :- This defines a interrupt priority range. All application interrupts whose priority is more than or equal to this level will be disabled during an EtherCAT interrupt service routine execution.
- Ethercat EEPROM Emulation Enabled :- EEPROM Emulation is enabled for this device to work with TwinCAT manager.
- Following table maps EtherCAT interrupt name with respective peripheral
channel selection. EIC interrupt handler and the SPI chip select
Configuration for EVB_LAN9255_SAME53
Interrupt Name EIC Channel SYNC0 Interrupt EIC_EXTINT0 SYNC1 Interrupt EIC_EXTINT1 IRQ Interrupt EIC_EXTINT7 Other Usage Port Pin SPI Chip Select PORT RB11 Error Select Pin PORT RB31
Note: EIC/GPIO/PIO pins for external event registration and event handler processing can be selected based on the microcontroller and LAN9255 interrupt support.SPI Configuration Mode Supported Description ETHERCAT_SPI_INDIRECT_MODE_ACCESS SPI Indirect Mode ETHERCAT_SPI_DIRECT_MODE_ACCESS SPI Direct Mode ETHERCAT_SPI_BECKHOFF_MODE_ACCESS SPI Beckhoff Mode - EIC, QSPI and TC0 are configured as per the application requirement.
- These are the below PINs configured for the application
- QSPI PIN Configuration for EVB_LAN9255_SAME53
QSPI Custom Name Function PORT PIN ID QSPI_MOSI QSPI_DATA0 PA08 QSPI_MISO QSPI_DATA1 PA09 QSPI_SCK QSPI_SCK PB10 SPI_CS GPIO PB11 - PIN Configuration for EtherCAT External Interrupt Pins for
EVB_LAN9255_SAME53
EIC Custom Name EIC Channel Port Pin EIC_EXTINT0 EIC_EXTINT0 PORT PB16 EIC_EXTINT1 EIC_EXTINT1 PORT PB17 EIC_EXTINT7 EIC_EXTINT7 PORT PB23
- QSPI PIN Configuration for EVB_LAN9255_SAME53
- Open NVIC configuration window from MHC→Tools. Set the QSPI Interrupt Priority Level to 2. This interrupt priority level is selected to be less than value of the EtherCAT Interrupt Priority Level configuration option in the LAN9255 component.
- The application will use the default clock options. No changes are required in clock settings.
- The FoE application uses a customized linker file. The ROM_LENGTH
attribute in the linker file is modified to 0x80000 for LAN9255ZMX020
(ATSAME53J20A). Bank A memory range is configured from 0x00000 to 0x7FFFF. Bank
B memory range is configured from 0x80000 to 0xFFFFF.
- The Dual Bank feature enables the FoE firmware to be executed from one bank while an updated version of the firmware is programmed into the other bank. The APP_BankSwitch() application function is called to swap the banks and to reset the device when the programming is complete. The APP_RunApplication() function is called to execute the new firmware.
- EEPROM Emulation starts from 0x3E000 (EEPROM_ORIGIN) and total length is 2000.
- To add a customized linker file to the project, uncheck the Add linker file to project option. Navigate to System>Project Configuration>Tool Chain Selections>Add linker file in the MHC Project graph to add the customized linked script file.
See the below screen shots: - Generate the code by clicking the Generate Code button (marked in red).
- The following diagram shows the generated EtherCAT project. This contains the sample_app.c file. It does not contain Beckhoff Client stack code. The Beckhoff Client Stack Code should be generated using the SSC tool with the required configuration and the Microchip-SAME53-EtherCAT-Slave_SSC_Config_SPI_< direct/indirect/beckhoff >_mode.xml file. The folder view on the right side in the below figure shows the EtherCAT project with SSC stack files added to the folder.
Completing The EtherCAT Application
This section demonstrates the MPLAB® X IDE projects for the ethercat_counter_foe_app application. The following table list the MPLAB® X projects available for the demonstration. These projects are available inside < install-dir >/ethercat/apps/ethercat_counter_foe_app/firmware.
- MPLAB® X project table
Project Name Target Device Target Development board Description SAME53_lan9255_evb.X LAN9255ZMX020 EVB-LAN9255_SAME53 ETherCAT evaluation board with LAN9255 with SPI Communication - The project contains the MPLAB® Harmony components that are required for an
EtherCAT application. The application files need to be added to the
project.
The application source files for the ethercat_counter_foe_app which are available in Harmony_Repo_Path/h3/ethercat/apps/ethercat_counter_foe_app/firmware/src.
- The app_lan9255.c, app_lan9255.h, main.c files are updated to demonstrate the application.
- The apps/ethercat_counter_foe_app/firmware/src/config/SAME53_lan9255_evb/ethercat_foe.ld linker file is a modified linker file which is used for FOE application.
- The sample application files eeprom.h, sample_app.c,
sample_app.h and sample_appObjects.h, generated by SSC tool,
are updated for the application requirement.
The SSC tool generated sample application files, highlighted in the above screen capture above, are updated for Counter, Trigger peripheral interface and for the FoE read/write operations. These are available in the apps/ethercat_counter_foe_app/firmware/src/slave_stack folder.
- Verify the XC32 Compiler Toolchain version and set the Connected Hardware Tool to ICD4 or PICkit 3. Press Apply button and then press OK button.
- Build the application by clicking on the Build Main Project.
Running the Application
TwinCAT Manager and Microchip EtherCAT Client communication
ETHERCAT INTERFACE DETECT AND EEPROM PROGRAMMING
- Upon successful installation of the TwinCAT Manager, the network adapter
will be moved to Installed and ready to use devices section as shown in
the following figure.
Please find the below table for the available Client configuration files which are generated by SSC tool.
Client Configuration File Mode SAME53_SPI_Indirect_Mode.xml SPI Indirect mode SAME53_SPI_Direct_mode.xml SPI Direct mode MSAME53_SPI_Beckhoff_mode.xml SPI Beckhoff mode - Default EEPROM Emulation is enabled for the EVB-LAN9255_SAME53
evaluation board. The strap along with EE_EMULI1 and EE_EMUL2 configures
the default PDI selection during EEPROM Emulation mode.
- Jumper Settings as per the different modes -
- Indirect mode
Jumper (J17) Description Configuration JP3 EE_MUL0 0 and 1 connected JP4 EE_MUL0 0 and 1 connected JP5 EE_MUL1 0 and 1 connected JP5 EE_MUL2 0 and 1 connected - Direct mode
Jumper (J17) Description Configuration JP3 EE_MUL0 0 and 1 connected JP4 EE_MUL0 0 and 1 connected JP5 EE_MUL1 0 and 1 connected JP5 EE_MUL2 1 and 2 connected
- Indirect mode
- Jumper Settings as per the different modes -
- In TwinCAT XAE, create a New Project (File=>New=>Project). In the New Project Window, select the TwinCAT Projects option and then click OK
- Connect port zero (J1 connector) of the EVB_LAN9255_SAME53 board to the TwinCAT Manager using a RJ45 Ethernet cable, and then power up the board. The Link/Act LED should be ON at Port zero when the cable is connected. If the Link/Act LED is not ON, then this indicates that there is an issue with the connection or the cable.
- Expand the IO option in the TwinCAT XAE project window and right click on Devices. Select Scan.
- Click OK if the TwinCAT network interface is selected and continue scanning as shown in the below image.
- Click OK to continue scanning and Click Yes in the Scan for boxes prompt.
- EEPROM Programming After a successful scan, click on Device 2 (EtherCAT) in the solution explorer window of the TwinCAT tool and Click Online in the TwinCAT project window. Once this is done, highlight the Device. This should read OP.
TRIGGER AND COUNTER DEMONSTRATION
This section describes the Tigger ( Output value for the TwinCAT manager and Input value to the LAN9255 EtherCAT device ) parameter and the Counter (Input value to the TwinCAT manager and Output value for the LAn9255 EtherCAT device ) parameter configuration. Counter parameter value is determined based on Trigger parameter value. If Trigger parameter value is 0, then Counter parameter is cleared. Trigger parameter value is used to determine value of Counter parameter.
- Input Trigger configuration - From I/O level on the Solution Explorer (left window), go to Devices=>Device # (EtherCAT)=>Box 1 (SAME53 EtherCAT Client)=>Outputs process data mapping=>Trigger.
- To change the Trigger parameter value, click on the Trigger which is available under Output process data mapping in the Search Solution Explorer window. In the top center window, select Online tab. Click Write and then enter 1 in Decimal: field and click OK.( Trigger parameter value can be anything. The default Trigger parameter value is used here).
- Output Counter Observation - From I/O level on the Solution Explorer (left window), go to Devices=>Device # (EtherCAT)=>Box 1 (SAME53 EtherCAT Client)=>Inputs process data mapping=>Counter.
- The Counter parameter value will be incremented based on the Trigger value. ( The Counter value will not be a stable value and will keep incrementing based on the Trigger value. ) In the top center window, select Online tab.
FILE OVER ETHERCAT COMMUNICATION
- FoE (File over EtherCAT) Test Update - Click on Box1, Select “Online” tab. Before FoE test Curent state and Requested state should be in OP mode.
- For file download, change the mode from INIT to BOOT mode.
- After clicking Download button , select BIN file that need
to be downloaded and configure the Password as per the
EtherCAT component password configuration.
The sample BIN files are present in < harmony-repo >/ethercat/apps/ethercat_counter_foe_app/firmware/src/FoE_Bin_imagefiles/lan9252_foe_binfiles folder can be used to verify the operation of the FoE application.
Note: A BIN file can be generated from the generated EtheCAT HEX image after configuring the Project Properties->Conf:->Building->Execute This Line After Build ${MP_CC_DIR}/xc32-objcopy” -I ihex -O binary “${DISTDIR}/${PROJECTNAME}.${IMAGE_TYPE}.hex” “${DISTDIR}/${PROJECTNAME}.${IMAGE_TYPE}.bin.Note: The Execute This Line After Build option should be unchecked in debug mode. - The download process can be tracked as shown in the figure below.
- After successful download, change the state from BOOT to INIT mode. This helps the application switch the bank from BANK B to BANK A and the newly downloaded firmware will be executed from BANK A. The new application starts running from flash location 0x0.