1.2.3 EtherCAT Counter-Trigger and FoE Application for EVM_LAN9253_SAMD51 SQI Communication
This EtherCAT example application demonstrates Counter-Trigger and Firmware Update over EtherCAT capability with SQI communication. The Counter and Trigger parameters are configured in the < ethercat repo >/apps/ethercat_counter_foe_app/firmware/src/slave_stack/lan9253 and demonstrates the communication between the EtherCAT Manager (TwinCAT Manager) and the EtherCAT Client (EtherCAT LAN9253).The firmware update is performed by FoE (File over EtherCAT) protocol. It is triggered by the EtherCAT Manager (TwinCAT Manager) which then download the firmware onto the EtherCAT Client (EtherCAT LAN9253) communication with EVB_LAN9253_SAMD51 board.
This demonstration help document contains the following sections:
- MPLAB® Harmony Software Setup
- Hardware Setup
- Beckhoff Client Stack Code (SSC) Generation
- MPLAB® Harmony Project configuration
- Completing The EtherCAT Application
- Running The Application
- TwinCAT Manager and Microchip EtherCAT Client communication
- EtherCAT interface detect and EEPROM Programming
- Trigger and Counter Demonstration
- File over EtherCAT communication
- TwinCAT Manager and Microchip EtherCAT Client communication
MPLAB® Harmony Software Setup
The following MPLAB® software components are a prerequisite for the rest of the steps in this demonstration. Please follow the download and installation instructions available at below links.
- MPLAB® X Integrated Development Environment
- MPLAB® XC32/32++ C Compiler
- MPLAB® Harmony Configurator
- On the management PC, download and Install on the TwinCAT 3 Engineering Full Setup at https://www.beckhoff.com/english.asp?download/tc3-download-xae.htm. Select the latest TwinCAT 3.1 Version and click on the link. Note the dialog box shows the TwinCAT tool that will be installed TC31-Full-Setup.3.1.XXXX.XX and click on “Start Download”. Follow instructions to download.
Hardware Setup
The following tools will be used to program and debug the application on the target hardware.
- MPLAB® ICD4 + ICD4/PICKIT 3 Target Adapter Board using JTAG interface.
The following development board will be used for EtherCAT application development and run the application.
- LAN9253 - EtherCAT Client Controller
evaluation kit with SAMD51 Microcontroller
The instructions in this guide are also applicable to other development boards with LAN9253 EtherCAT Client device. Hardware settings are board dependent and may vary between boards.
- Connect a micro USB cable to J8 port for power source.
- For programming, Connect a ICD4 JTAG cable to the J10 port of the EVB_LAN9253_SAMD51 board.
- Connect RJ45 connector J1 to the TwinCAT Manager.
- Block diagram of the EVB_LAN9253_SAMD51 board
Beckhoff Client Stack Code (SSC) Generation
Follow instruction at this link to generate Beckhoff Client Stack Code: Steps to generate Beckhoff Client Stack Code.
MPLAB® Harmony Project Configuration
There are two options available for downloading/installing the MPLAB® Harmony Software Repositories from github & gitee.
The required repositories can be cloned from the github (or gitee) by using a local git client (such git bash). The MPLAB® Harmony Repositories are available at the following links:
https://github.com/Microchip-MPLAB-Harmony/
https://gitee.com/Microchip-MPLAB-Harmony/
The csp, dev_packs, mhc and ethercat repositories should be cloned. The required repositories can also be cloned (downloaded) or previously downloaded repositories can be updated by using the MPLAB® Harmony 3 Content Manager. The following sections provide details on using the MPLAB® Harmony 3 Content Manager to download the repositories.
- Refer to the EtherCAT MPLAB® Harmony Software Setup https://github.com/Microchip-MPLAB-Harmony/ethercat/wiki/create-your-first-ethercat-application details to create a EtherCAT project.
- The following Project Graph diagram shows the required Harmony components those are included for the present EtherCAT application for the EVB_LAN9253_SAMD51 board with sqi communication.
- Click on the EtherCAT Stack in
the Project Graph window. In the Configuration window,
- The Beckhoff Client Stack source directory path should point to the folder that contains the files generated by the SSC tool.
- Enable FoE checkbox enables File over EtherCAT feature.
- Click on LAN9253 component
from the project graph.
- EtherCAT Interrupt Priority Level :- This defines a interrupt priority range. All application interrupts whose priority is more than or equal to this level will be disabled during an EtherCAT interrupt service routine execution.
- Following table maps
EtherCAT interrupt name with respective peripheral channel selection.
EIC interrupt handler and the Error Pin Configuration for
EVB_LAN9253_SAMD51
Interrupt Name EIC Channel SYNC0 Interrupt EIC_EXTINT0 SYNC1 Interrupt EIC_EXTINT1 IRQ Interrupt EIC_EXTINT7 Other Usage Port Pin Error Select Pin PORT RB31
Note: EIC/GPIO/PIO pins for external event registration and event handler processing can be selected based on the microcontroller and LAN9253 interrupt support.SQI Cofiguration Mode Supported Description ETHERCAT_SQI_INDIRECT_MODE_ACCESS SQI Indirect Mode ETHERCAT_SQI_DIRECT_MODE_ACCESS SQI Direct Mode - EIC, QSPI and TC0 are configured as per the application requirement.
- These are the below PINs
configured for the application
- QSPI PIN Configuration
for EVB_LAN9253_SAMD51
QSPI Custom Name Function PORT PIN ID QSPI_DATA0 QSPI_DATA0 PA08 QSPI_DATA1 QSPI_DATA1 PA09 QSPI_DATA2 QSPI_DATA1 PA10 QSPI_DATA3 QSPI_DATA3 PA11 QSPI_SCK QSPI_SCK PB10 QSPI_CS QSPI_CS PB11 - PIN Configuration for
EtherCAT External Interrupt Pins for EVB_LAN9253_SAMD51
EIC Custom Name EIC Channel Port Pin EIC_EXTINT0 EIC_EXTINT0 PORT PB16 EIC_EXTINT1 EIC_EXTINT1 PORT PB17 EIC_EXTINT7 EIC_EXTINT7 PORT PB23
- QSPI PIN Configuration
for EVB_LAN9253_SAMD51
- The application will use the default clock options. No changes are required in clock settings.
- The FoE application uses a
customized linker file. The ROM_LENGTH attribute in the linker file is
modified to 0x40000 for ATSAMD51J19A. Bank A memory range is configured from
0x00000 to 0x3FFFF. Bank B memory range is configured from 0x40000 to
0x7FFFF.
The Dual Bank feature enables the FoE firmware to be executed from one bank while an updated version of the firmware is programmed into the other bank. The APP_BankSwitch() application function is called to swap the banks and to reset the device when the programming is complete. The APP_RunApplication() function is called to execute the new firmware.
To add a customized linker file to the project, uncheck the Add linker file to project option. Navigate to System>Project Configuration>Tool Chain Selections>Add linker file in the MHC Project graph to add the customized linked script file.
See the below screen shots: - Generate the code by clicking the Generate Code button.
- The following diagram shows the generated EtherCAT project. This contains the sample_app.c file. It does not contain Beckhoff Client stack code. The Beckhoff Client Stack Code should be generated using the SSC tool with the required configuration and the Microchip-SAMD51-EtherCAT-Slave_SSC_Config_SQI_< direct/indirect/beckhoff >_mode.xml file. The folder view on the right side in the below figure shows the EtherCAT project with SSC stack files added to the folder.
Completing The EtherCAT Application
This section demonstrates the MPLAB® X IDE projects for the ethercat_counter_foe_app application. The following table list the MPLAB® X projects available for the demonstration. These projects are available inside < install-dir >/ethercat/apps/ethercat_counter_foe_app/firmware .
- MPLAB® X project table
Project Name Target Device Target Development Board Description samd51_lan9253_evb_sqi.X ATSAMD51J19A EVB-LAN9253_SAMD51 ETherCAT evaluation board with LAN9253 SQI Communication - The project contains the MPLAB® Harmony components that are required for an
EtherCAT application. The application files need to be added to the
project.
The application source files for the ethercat_counter_foe_app which are available in Harmony_Repo_Path/h3/ethercat/apps/ethercat_counter_foe_app/firmware/src.
- The app_lan9253.c, app.h, main.c files are updated to demonstrate the application.
- The apps/ethercat_counter_foe_app/firmware/src/config/samd51_lan9253_evb/ethercat_foe.ld linker file is a modified linker file which is used for FOE application.
- The sample application files sample_app.c, sample_app.h and
sample_appObjects.h, generated by SSC tool, are updated for the
application requirement.
The SSC tool generated sample application files, highlighted in the above screen capture above, are updated for Counter, Trigger peripheral interface and for the FoE read/write operations. These are available in the apps/ethercat_counter_foe_app/firmware/src/slave_stack folder.
- Verify the XC32 Compiler Toolchain version and set the Connected Hardware Tool to ICD4 or PICkit 3. Press Apply button and then press OK button.
- Build the application by clicking on the Build Main Project.
Running the Application
TwinCAT Manager and Microchip EtherCAT Client communication
ETHERCAT INTERFACE DETECT AND EEPROM PROGRAMMING
- Upon successful installation of the TwinCAT Manager, the network adapter
will be moved to Installed and ready to use devices section as shown in
the following figure.
Please find the below table for the available Client configuration files which are generated by SSC tool.
Client Configuration File Mode SAMD51_SQI_Indirect_Mode.xml SPI Indirect mode SAMD51_SQI_Direct_mode.xml SPI Direct mode Copy the required available configuration file from < harmony-repo >/ethercat/slave_stack/lan9253/ directory to the TwinCAT\3.1\Config\Io\EtherCAT directory.
- In TwinCAT XAE, create a New Project (File=>New=>Project). In the New Project Window, select the TwinCAT Projects option and then click OK.
- Connect port zero (J1 connector) of the EVB_LAN9253_SAMD51 board to the TwinCAT Manager using a RJ45 Ethernet cable, and then power up the board. The Link/Act LED should be ON at Port zero when the cable is connected. If the Link/Act LED is not ON, then this indicates that there is an issue with the connection or the cable.
- Expand the IO option in the TwinCAT XAE project window and right click on Devices. Select Scan.
- Click OK if the TwinCAT network interface is selected and continue scanning as shown in the below image.
- Click OK to continue scanning and Click Yes in the Scan for boxes prompt.
- EEPROM Programming After a successful scan, click on Device 2 (EtherCAT) in the solution explorer window of the TwinCAT tool and Click Online in the TwinCAT project window. Once this is done, highlight the Device. This should read OP.
TRIGGER AND COUNTER DEMONSTRATION
This section describes the Tigger ( Output value for the TwinCAT manager and Input value to the LAN9253 EtherCAT device ) parameter and the Counter (Input value to the TwinCAT manager and Output value for the LAn9253 EtherCAT device ) parameter configuration. Counter parameter value is determined based on Trigger parameter value. If Trigger parameter value is 0, then Counter parameter is cleared. Trigger parameter value is used to determine value of Counter parameter.
- Input Trigger configuration - From I/O level on the Solution Explorer (left window), go to Devices=>Device # (EtherCAT)=>Box 1 (SAMD51 EtherCAT Client)=>Outputs process data mapping=>Trigger.
- To change the Trigger parameter value, click on the Trigger which is available under Output process data mapping in the Search Solution Explorer window. In the top center window, select Online tab. Click Write and then enter 1 in Decimal: field and click OK.( Trigger parameter value can be anything. The default Trigger parameter value is used here).
- Output Counter Observation - From I/O level on the Solution Explorer (left window), go to Devices=>Device # (EtherCAT)=>Box 1 (SAMD51 EtherCAT Client)=>Inputs process data mapping=>Counter.
- The Counter parameter value will be incremented based on the Trigger value. ( The Counter value will not be a stable value and will keep incrementing based on the Trigger value. ) In the top center window, select Online tab.
FILE OVER ETHERCAT COMMUNICATION
- FoE (File over EtherCAT) Test Update - Click on Box1, Select “Online” tab. Before FoE test Curent state and Requested state should be in OP mode.
- For file download, change the mode from INIT to BOOT mode.
- After clicking Download button , select BIN file that need
to be downloaded and configure the Password as per the
EtherCAT component password configuration.
The sample BIN files are present in < harmony-repo >/ethercat/apps/ethercat_counter_foe_app/firmware/src/FoE_Bin_imagefiles/lan9253_foe_binfiles folder can be used to verify the operation of the FoE application.
Note: A BIN file can be generated from the generated EtheCAT HEX image after configuring the Project Properties->Conf:->Building->Execute This Line After Build ${MP_CC_DIR}/xc32-objcopy” -I ihex -O binary “${DISTDIR}/${PROJECTNAME}.${IMAGE_TYPE}.hex” “${DISTDIR}/${PROJECTNAME}.${IMAGE_TYPE}.bin.Note: The Execute This Line After Build option should be unchecked in debug mode. - The download process can be tracked as shown in the figure below:
- After successful download, change the state from BOOT to INIT mode. This helps the application switch the bank from BANK B to BANK A and the newly downloaded firmware will be executed from BANK A. The new application starts running from flash location 0x0.