2.6 Remote Command Configuration
This section describes the procedure required to demonstrate the RNBD350 remote command feature. This feature allows the control of an RNBD350 module without the use of a host microcontroller remotely from another RNBD350 module.
The remote command feature works by using a special BLE GATT service that emulates a wireless serial connection called transparent UART mode. This combined with a unique command set allows remote functionality of the module.
The remote command feature can be controlled by RNBD350 module.
For the first demonstration, two RNBD350 modules will be used. One will be called the Controller Module and the other will be Remote Module. The Controller Module is connected to the PC and is in control of the Remote Module. The Remote Module is connected to the PC for the status feedback.
Remote RNBD350 Module Configuration
Follow the below steps to configure the remote module
Step 1 ––– Enter command mode
Input Command: $$$
Expected response:CMD>
Step 2 ––- Set to Factory defaults
Input Command:SF,1<CR><LF>
Expected response: Reboot after Factory
Reset<CR><LF>
%REBOOT%
Step 3 –– Enter command mode
Input Command: $$$
Expected response: CMD>
Step 4 –– Set name of module to "Remote"
Input Command:SN,Remote<CR><LF>
Expected response : AOK<CR><LF>
CMD>
Step 5 –– Enable device information and transparent and UART operation
Input Command: SS,C0<CR><LF>
Expected response : AOK<CR><LF>
CMD>
Step 6 –– Enable authentication/security
Input Command:SA,2,<CR><LF>
Expected response:
AOK<CR><LF>
CMD>
Step 7 –– Set 4 digit PIN code
Input Command:SP,1234<CR><LF>
Expected response: AOK<CR><LF>
CMD>
Step 8 –– Save and reboot
Input Command:R,1<CR><LF>
Expected response:
Rebooting<CR><LF>
%REBOOT%
Controller RNBD350 Module Configuration
Follow the below steps to configure the controller module
Step 1 ––– Enter command mode
Input Command: $$$
Expected response:CMD>
Step 2 ––- Set to Factory defaults
Input Command:SF,1<CR><LF>
Expected response: Reboot after Factory
Reset<CR><LF>
%REBOOT%
Step 3 –– Enter command mode
Input Command: $$$
Expected response: CMD>
Step 4 –– Set name of module to "Controller"
Input Command:SN,Controller<CR><LF>
Expected response : AOK<CR><LF>
CMD>
Step 5 –– Enable device information and transparent and UART operation
Input Command: SS,C0<CR><LF>
Expected response : AOK<CR><LF>
CMD>
Step 6 –– Enable authentication/security
Input Command:SA,2,<CR><LF>
Expected response: AOK<CR><LF>
CMD>
Step 7 –– Set 4 digit PIN code
Input Command:SP,1234<CR><LF>
Expected response: AOK<CR><LF>
CMD>
Step 8 –– Save and reboot
Input Command:R,1<CR><LF>
Expected response: Rebooting<CR><LF>
%REBOOT%
Step 9 ––– Enter command mode
Input Command: $$$
Expected response:CMD>
Step 10 ––- Enter command to connect to the Remote module.
Input Command: C,0,<BDA><CR><LF>
Expected response:
%CONNECT,0,xxxxxxxxxxxx,0071%%PHY_UPDATED,0071,02,02%%NOTI,0057,001400F710%%STREAM_OPEN%
Step 11 –- Enter command mode
Input Command: $$$
Expected response:CMD>
Step 12 –- Issue Bonding
Input Command: B<CR><LF>
Expected response: AOK<CR><LF>
CMD< %BONDED%%SECURED%
Step 13 –– Enter remote command mode
Input Command: !,1<CR><LF>
Expected Response: RMT>
Now the the RNBD350 Controller Module is in Remote Command mode of the RNBD350 Remote Module.
Remote Command mode testing
Now with the above steps the remote command mode is successfully configured.
Now lets try to control the RNBD350 Remote module with some sample example sections
Example 1
In this example the remote RNBD350 module will "Dump" its information like BDA Address, the module name, connection status, security settings,Enabled features and enabled services
Input Command: D<CR><LF>
Expected Resposne: BTA=3481F4AE0EA8
Name=Remote
Connected=FC0FE7801521,0
Authen=2
Features=0000
Services=C0
RMT>
Example 2
In this example the name of RNBD350 remote module will be returend to the Controller Module.
Input Command: GN<CR><LF>
Expected Resposne: Remote
RMT>
Example 3
In this example the firmware version of RNBD350 remote module will be returend to the Controller Module.
Input Command: V<CR><LF>
Expected Resposne: RNBD350 V1.0.0.10
Jul 20 2022 (c)Microchip Technology Inc
RMT>
NOTE: To exit Remote Command mode
Input Command: $$$
Expected response:CMD>
The CMD>indicate the remote command mode is turned off and the
RNBD350 Controller device entered into
command mode.