2 Application Demo Scenarios
This chapter describes a few application use cases about how to control the RNBD350 module and connect it with peer Bluetooth devices (mobile phone). All the demo scenarios use a PC to connect with the RNBD350 module as host emulation system. The RNBD350 Add On Board from Microchip has the UART-to-USB converter that can be connected with a PC tool. Though the demo steps explain using an emulated host environment (PC based), the procedure is applicable for the RNBD350 module connected to the host MCU as well, where the host MCU must send the command to the RNBD350 module instead of the PC.