3.6.2 Constraints Manual

Learn more about the constraints available for SmartHLS.

3.6.2.1 Constraints Manual

SmartHLS accepts user-provided constraints that impact the automatically generated hardware. These constraints can be specified using the SmartHLS IDEand are stored in the Tcl configuration file config.tcl located in your project directory. This section provides information about the constraints available for SmartHLS. The main constraints available from the SmartHLS IDE are:

A few debugging constraints are available from the SmartHLS IDE:

3.6.2.2 Commonly Used Constraints

3.6.2.2.1 CLOCK_PERIOD

This is a widely used constraint that allows the user to set the target clock period for a design. The clock period is specified in nanoseconds.

It has a significant impact on scheduling: the scheduler will schedule operators into clock cycles using delay estimates for each operator, such that the specified clock period is honored. In other words, operators will be chained together combinationally to the extent allowed by the value of the CLOCK_PERIOD parameter.

SmartHLS has a default CLOCK_PERIOD value for each device family that is supported (see table in SmartHLS Constraints).

Category
HLS Constraints
Value Type
Decimal or integer; represents a value in nanoseconds
Valid Values
Positive decimal or positive integer
Default Value
Depends on the target device
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter CLOCK_PERIOD 15

3.6.2.2.2 SINGLE_HDL_OUTPUT_FILE

When set to 1, this Tcl parameter constrains SmartHLS-generated Verilog RTL and VHDL wrapper modules to a single Verilog file (<Project Name>.v) and a single VHDL file (<Project Name>.vhd) respectively. By default, each Verilog top-level module (and its child modules) is printed to a separate output file (<Project Name>_<Top-Level Name>.v), and each VHDL wrapper module of a top-level is printed to a separate VHDL file (<Project Name>_<Top-Level Name>.vhd).

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
SINGLE_HDL_OUTPUT_FILE 0
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter SINGLE_HDL_OUTPUT_FILE 1

3.6.2.2.3 set_custom_config_file

If you want to add advanced SmartHLS Tcl constraints that are not listed in the SmartHLS IDE constraints dialog you need to use a custom config file. Be careful not to modify the config.tcl constraints file directly, since config.tcl will be overwritten whenever you make changes in the SmartHLSIDE constraints dialog.

To add a custom config file:
  1. Open the SmartHLS Constraints Menu.
  2. Select Set custom config file from the dropdown and enter the Constraint Value as "custom_config.tcl".
  3. Click Add:
  4. Now click OK:

  5. Now in the Project Explorer, right click and select New > File:

  6. Enter the name of "custom_config.tcl". This should match the file name entered in the Set HLS Constraints previously. Click Finish:

3.6.2.2.4 set_custom_test_bench_file

This Tcl command is to specify the user-provided custom testbench file that defines the custom testbench module, which is set via set_custom_test_bench_module. This is not needed for SW/HW co-simulation.

Category
Simulation
Value Type
String
Dependencies
set_custom_test_bench_module "user_tb"
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_custom_test_bench_file user_tb.v

3.6.2.2.5 set_custom_test_bench_module

This Tcl command is to specify the name of the user-provided testbench module to be using for RTL simulation. The testbench file must also be specified withset_custom_test_bench_file .

Category
Simulation
Value Type
String
Dependencies
set_custom_test_bench_file user_tb.v
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_custom_test_bench_module "user_tb"

3.6.2.2.6 set_operation_latency

This Tcl command sets the latency of a given operation.Latency refers to the number of clock cycles required to complete the computation; an operation with latency one requires one cycle, while zero-latency operations are completely combinational, meaning multiple such operations can be chained together in a single clock cycle. This command is used to schedule each type operation to take the specified number of cycles.

This Tcl command should only be used by advanced SmartHLS users.

Category
HLS Constraints
Value Type
set_operation_latency <operation> <constraint>, in which <operation> is a string and <constraint> is an integer
Valid Values
See Default and Examples.
Note: Operator name should match the operation database file: devices/Microchip.tcl or devices/set_operation_latency.tcl

See ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING for information on default latency for memory latency.

See FORCED_MATH_BLOCK_PIPELINE_DEPTH for information on latency control per Math (DSP) block.

Default Values
fp_add_64 12
fp_add_32 11
fp_subtract_64 12
fp_subtract_32 11
fp_multiply_64 8
fp_multiply_32 5
fp_divide_32 33
fp_divide_64 61
fp_truncate_64 5
fp_extend_32 4
fp_signed_comp_o 3
fp_signed_comp_u 3
fp_sitofp_32_32 4
fp_sitofp_32_64 5
fp_sitofp_64_32 5
fp_sitofp_64_64 5
fp_uitofp_32_32 4
fp_uitofp_32_64 4
fp_uitofp_64_32 5
fp_uitofp_64_64 4
fp_fptosi_32_32 4
fp_fptosi_32_64 5
fp_fptosi_64_32 4
fp_fptosi_64_64 5
fp_fptoui_32_32 4
fp_fptoui_32_64 5
fp_fptoui_64_32 4
fp_fptoui_64_64 5
reg 2
external_memory_port 1
Location Where Default is Specified
devices/Microchip.tcl

and

devices/set_operation_latency.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
# set memory operations to take 3 cycles
set_operation_latency memory_port 3

3.6.2.2.7 set_project

This parameter sets the default target project, or device, used. Changing the project also updates the associated family and board parameters.

This parameter has 3 arguments:

  • FPGA Family (e.g. PolarFire®).
  • FPGA Device: This can either be the board name (e.g. MPF300), or the device number (e.g. MPF300TS-1FCG1152I).
  • Flow: hw_only, Icicle_SoC or MiV_SoC.
    • hw_only: SmartHLS only generates an IP core.
    • Icicle_SoC: SmartHLS SoC commands generate a reference design targeting the PolarFire® SoC Icicle kit devices.
    • MiV_SoC: SmartHLS SoC commands generate a MiV RV32 reference design targeting the PolarFire® Video Kit board.
Category
Board and Device Specification
Value Type
String
Valid Values
See Examples
Default Value
PolarFire MPF300 hw_only
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_project PolarFire MPF300 hw_only
set_project PolarFire MPF300T-1FCG1152I hw_only
set_project SmartFusion2 FUTUREM2SF hw_only
set_project SmartFusion2 M2S025T-FG484I hw_only
set_project IGLOO2 M2GL005-1FG484 hw_only

3.6.2.2.8 set_resource_constraint

This Tcl command constrains the resource allocated by SmartHLS. For instance, to only have a single divider in the entire circuit, user can specify: set_resource_constraint divide 1. This makes SmartHLS instantiate a maximum of 1 divider in the circuit, and if there are multiple division operations required, they will share the same divider.

Important: A constraint on "divide" will apply to:
  • signed_divide_8
  • signed_divide_16
  • signed_divide_32
  • signed_divide_64
  • unsigned_divide_8
  • unsigned_divide_16
  • unsigned_divide_32
  • unsigned_divide_64

It can also be used to constrain the number of memory ports. To make all memories single-ported: set_resource_constraint memory_port 1 For memory ports, only 1 and 2 are valid values, as FPGA RAMs have up to 2 ports.

This Tcl command should only be used by advanced SmartHLS users.

Category
HLS Constraints
Value Type
set_resource_constraint <operation> <constraint>, in which <operation> is a string and <constraint> is an integer
Valid Values
See Default and Examples
Important: Operator name should match the device family operation database file: boards/PolarFire/PolarFire.tcl
Default Values
memory_port 2
divide 1
modulus 1
fp_add 1
fp_subtract 1
fp_multiply 1
fp_divide 1
fp_truncate 1
fp_extend 1
fp_fptosi 1
fp_sitofp 1
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_resource_constraint signed_divide_16 3
set_resource_constraint signed_divide 2
set_resource_constraint divide 1
Important:

The multiply splitting feature (see ENABLE_MULTIPLY_SPLITTING) does not support multiplier sharing. Therefore, if a user specifies set_resource_constraint multiply X, multiplication splitting will be disabled, regardless of the value set to ENABLE_MULTIPLY_SPLITTING. In such cases, SmartHLS will issue a warning message: Warning: Detected set_resource_constraint setting for integer multiplier. However, multiplier sharing is incompatible with the multiply splitting feature. Disabling multiply splitting feature and the normal multiplier modules will be used.

In this case, the latency of all multiplication operations will be determined by the value set in the set_operation_latency multiply X command. If this command is not used, latency will default to 2.

3.6.2.2.9 set_synthesis_top_module

This Tcl command specifies the name of the Verilog module that will be set as the top-level module when creating a Libero project for synthesis, place and route. By default, the top-level function (see Specifying the Top-level Function) is set as the top-level module for the Libero project, however user may want to provide wrapper HDL module that instantiates the SmartHLS-generate top-level module. In this case, this Tcl command can be used to give the name of the wrapper module.

Category
Libero
Value Type
String
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_synthesis_top_module "wrapper_top"

3.6.2.2.10 set_synthesis_top_module_file

When set_synthesis_top_module is used to set a different wrapper module as the top-level for synthesis, place & route, use this command to specify the file that defines the wrapper module.

Category
Libero
Value Type
String
Dependencies
set_synthesis_top_module "wrapper_top"
Applicable Flows
All devices and flows
Test Status
Actively in use
Examples
set_synthesis_top_module_file custom_synthesis_top.v

3.6.2.3 Debugging Constraints

3.6.2.3.1 COSIM<INPUT|OUTPUT>_FIFO_STALL_PROB

The COSIM_INPUT_FIFO_STALL_PROB and COSIM_OUTPUT_FIFO_STALL_PROB parameters can be used to exercise halting data injecting to input FIFO or backpressuring the output FIFO during Simulate HLS Hardware (SW/HW Co-Simulation). When the parameter is set to a value between 1 and 99, representing the probablity to halt input FIFO or backpressure output FIFO, the SmartHLS-generated CoSimulation testbench will randomly halt the data injectiion to input FIFO or backpressure output FIFO, which will then cause the SmartHLS-generated circuit to stall during simulation.

Category
HLS Constraint
Value Type
Integer
Valid Values
0-100
Default Value
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in use
Examples
set_parameter COSIM_INPUT_FIFO_STALL_PROB 50
set_parameter COSIM_OUTPUT_FIFO_STALL_PROB 40

3.6.2.3.2 KEEP_SIGNALS_WITH_NO_FANOUT

If this parameter is enabled, all signals will be printed to the output Verilog file, even if they don't drive any outputs.

Category
HLS Constraint
Value Type
Integer
Valid Values
0, 1
Default Value
0
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in use
Examples
set_parameter KEEP_SIGNALS_WITH_NO_FANOUT 1

3.6.2.3.3 VSIM_ASSERT

When set to 1, this constraint causes assertions to be inserted in the Verilog produced by SmartHLS. This is useful for debugging the circuit to see where invalid values (X's) are being assigned.

Category
Simulation
Value Type
Integer
Valid Values
0, 1
Default Value
0
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in use
Examples
set_parameter VSIM_ASSERT 1

3.6.2.4 Advanced Constraints

3.6.2.4.1 IFCONV_PREDICATE_LOADS

This constraint sets whether load instructions should be predicated during if-conversion. By default, it is set to 1 to predicate load instructions to avoid resource contention between mutually exclusive loads. If there is no resource contention between mutually exclusive loads, it can set to 0 avoid inserting predication logic.

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
1
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in use
Examples
set_parameter IFCONV_PREDICATE_LOADS 1

3.6.2.4.2 LATENCY_REDUCTION

The LATENCY_REDUCTION settings control the SmartHLS's expression balancing optimization, of which the objective is to reduce the circuit latency. Below are the related settings:

Parameter NameDefault ValueDescription
LATENCY_REDUCTION1The main switch that enables or disables expression balancing. Setting to 0 disables all expression balancing optimizations.
LATENCY_REDUCTION_ALLOW_FP_REORDERING0By default, expression balancing does not re-order floating-point operations to prevent loss of precisions.

Setting to 1 allows to re-order floating-point operations if the circuit latency can be reduced.

Because the floating point operations may lose their commutativity and associativity with finite precision, this optimization may result in the failure of the co-simulation.
CAUTION: This is an unsafe optimization. Users should only enable this option on error tolerant designs.
LATENCY_REDUCTION_REDUCE_FP_CONVERSIONS 0

Setting to 1 will allow SmartHLS to cancel out back-and-forth conversion between floating-point and integer, with potential variations in numerical values.

For example, the following conversions can be cancelled when this setting is 1.

int a = (int)(float)(3); // a == 3.

float b = (float)(int)(1.2); // b == 1.2 instead of 1.

Level of accuracy loss caused by this optimization is run-time value dependent. Therefore, carefully examine the potential value sets of the associated operations as well as your design tolerance before enabling this option.
CAUTION: This is an unsafe optimization. Users should only enable this option on error tolerant designs.
LATENCY_REDUCTION_BALANCE_MULTI_USE_NODE0

By default expression balancing does not optimize the intermediate operations that have multiple uses, to avoid potential increase of resource usage.

Setting to 1 allows to re-order intermediate operations that have multiple uses and more latency reduction could be achieved.

Category
HLS Constraints
Value Type
Integer
Valid Values
0, 1
Default Value
As listed in the table above.
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter LATENCY_REDUCTION 1
set_parameter LATENCY_REDUCTION_ALLOW_FP_REORDERING 0
set_parameter LATENCY_REDUCTION_REDUCE_FP_CONVERSIONS 0
set_parameter LATENCY_REDUCTION_BALANCE_MULTI_USE_NODE 0

3.6.2.4.3 ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING

Enable determining memory latency for reads automatically according to the target clock period and timing model of the board. Memory latency is set to 2 when the target clock period is less than the delay of memory for the target device, otherwise is set to 1. Increasing the memory latency can result in higher circuit Fmax at the expense of higher circuit latency. The auto-determined latency can be found in the Memory Usage section of SmartHLS report.

Setting the operation latency for a RAM will override the latency automatically calculated. See set_operation_latency for a list of valid memory port latency. The threshold for switching are listed in the table below.

Table 3-19. Thresholds for Switching
DeviceUse Memory Latency of 2 when Target Period is less than (ns)
PolarFire, PolarFire SoC4.167
IGLOO2, SmartFusion24.167
PolarFire 24.167

ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING controls the latency for the following memory constraints. Each constraint can be used with set_operation_latency <Name> <latency> to override the auto-determined latency.

Table 3-20. Memory Constraints Controlled by ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING
NameDescription
local_memory_portControls the memory latency of Local Memory used by a single function.
shared_local_memory_portControls the memory latency of Shared-Local Memory shared by multiple functions.
axi_slave_ram_memory_portControls the memory latency of Legacy AXI4 Slave Interface
memory_portControls the memory latency of Memory Controller

SmartHLS does not automatically determine the latency for external_memory_port as it is only for creating an interface with the RAMs outside of the circuit. However, for SmartHLS SoC Flow, external_memory_port controls the latency for the on-chip memory buffers.

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
1
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter ENABLE_AUTOMATIC_MEMORY_LATENCY_SETTING 1

3.6.2.4.4 ENABLE_MULTIPLY_SPLITTING

SmartHLS's default behavior is to map multiplication operations to Math blocks (DSPs). When a multiplication operation's width exceeds the maximum width that the target device's DSPs can support, SmartHLS automatically splits the operation across multiple DSPs. The internal pipeline registers within these DSPs are configured to meet the user-defined timing requirements (Fmax) while minimizing the execution latency or cycle count. Multiplication splitting is enabled by default and users have the option to disable it by setting this parameter to 0.
Category
HLS constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
1: enabled
Dependencies
None
Test Status
Actively in-use
Examples
set_parameter ENABLE_MULTIPLY_SPLITTING 0

3.6.2.4.5 FORCED_MATH_BLOCK_PIPELINE_DEPTH

Multipliers are implemented in Math (DSP) blocks. When this constraint is set to 0, the pipelining depth configuration, or latency, of each Math block is automatically calculated given the target clock frequency; the faster the clock, the deeper the pipeline. User can override the latency of each math block by setting FORCED_MATH_BLOCK_PIPELINE_DEPTH to a non-zero value, constrained by the target architecture.
Important: With ENABLE_AUTOMATIC_MULTIPLY_MODE_SETTING and MULTIPLY_SPLITTING_FULLY_PIPELINED removed since SmartHLS 2025.1, this constraint can be used to have more precise control of Math block pipelining depth.
Category
HLS Constraints
Value Type
Integer
Valid Values
0, 1, 2
Default Value
0
Dependencies
None
Test Status
Actively in use
Examples
set_parameter FORCED_MATH_BLOCK_PIPELINE_DEPTH 1

3.6.2.4.6 SOC_AXI_INITIATOR

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the AXI initiator interface used by the processor in the user-defined SmartDesign system to connect to the HLS module's AXI target interface. This AXI initiator interface is used by the processor to control and transfer data to/from the HLS modules.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on using this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
AXI2AXI_TO_HLS:AXI4_MASTER
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_AXI_INITIATOR AXI2AXI_TO_HLS:AXI4_MASTER

3.6.2.4.7 SOC_AXI_TARGET

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the AXI target interface in the user-defined SmartDesign system where the HLS module's AXI initiator interface can connect to. This AXI target interface is used by the HLS modules to access shared memory (DDR) directly.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on using this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
AXI2AXI_FROM_HLS:AXI4_SLAVE
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_AXI_TARGET AXI2AXI_FROM_HLS:AXI4_SLAVE

3.6.2.4.8 SOC_BD_NAME

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the SmartDesign system to integrate the HLS modules into.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
FIC_0_PERIPHERALS
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_BD_NAME FIC_0_PERIPHERALS

3.6.2.4.9 SOC_CLOCK

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the clock to connect to the HLS modules. Currently, all HLS modules use the same clock.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
ACLK
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_CLOCK ACLK

3.6.2.4.10 SOC_CPU_MEM_BASE_ADDRESS

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the base address of the memory window in the shared memory space (DDR) that can be accessed by the HLS module's AXI initiator interfaces. This address is used to configure the AXI interconnect that HLS modules connect to for accessing the shared memory.

Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Hexadecimal
Default Value (Based on Icicle SoC reference design)
0x80000000
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_CPU_MEM_BASE_ADDRESS 0x80000000

3.6.2.4.11 SOC_CPU_MEM_SIZE

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the size of the shared memory (DDR) space that the HLS module's AXI initiator interfaces can access.

Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Hexadecimal
Default Value (Based on Icicle SoC reference design)
0x60000000
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_CPU_MEM_SIZE 0x60000000

3.6.2.4.12 SOC_DMA_ENGINE

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the type of DMA engine to use in the system for transferring data to/from HLS modules.

DMA EngineDescription
HARD_DMAUses the DMA available in the PolarFire® SoC MSS. This implies that the CPUs to be used are the RISC-V U54 application cores in the MSS.
SOFT_DMA

Automatically instantiates a DMA engine on the FPGA fabric and be connected to the SmartHLS AXI interconnect along with the SmartHLS IP modules.

Currently this option is not enabled, but will be in a future release.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
HARD_DMA
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
HARD_DMA is actively in-use; SOFT_DMA will be made available in a future release
Examples
set_parameter SOC_DMA_ENGINE HARD_DMA

3.6.2.4.13 SOC_FABRIC_BASE_ADDRESS

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the base address of the CPU memory space that is reserved for all HLS modules. The control registers and on-chip memory buffers of HLS modules are allocated and mapped within this memory window. This address is also used to configure the AXI interconnect that HLS modules connect to.

Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Hexadecimal
Default Value (Based on Icicle SoC reference design)
0x70000000
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_FABRIC_BASE_ADDRESS 0x70000000

3.6.2.4.14 SOC_FABRIC_SIZE

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the size of the CPU memory space that is reserved for all HLS modules. The control registers and on-chip memory buffers of HLS modules are allocated and mapped within this memory window. This address is also used to configure the AXI interconnect that HLS modules connect to.

Note that the value for the parameter is specified in hexadecimal format and must be prefixed with 0x.

By default, 4MB of size is reserved. If this is larger than what HLS modules require, it can just be left for future use. Reserving a larger window does not mean more on-chip memory will be used.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Hexadecimal
Default Value (Based on Icicle SoC reference design)
0x400000
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_FABRIC_SIZE 0x400000

3.6.2.4.15 SOC_POLL_DELAY

This parameter controls how often an accelerator driver function polls the status register of an HLS module to check for its completion. By default, the delay is set to 0, which means the processor will continuously poll the status. However, it may be beneficial to insert a delay in polling to reduce CPU usage and power consumption. The poll delay is specified in microseconds.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
Integer; represents a value in microseconds
Valid Values
Non-negative integer
Default Value (Based on Icicle SoC reference design)
0
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_POLL_DELAY 10

3.6.2.4.16 SOC_PROFILER_COUNTER

This parameter specifies whether or not to include a hardware counter to help profile SoC-based designs. The counter is not included by default.

For more information, see SoC Profiler.

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
0
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_PROFILER_COUNTER 1

3.6.2.4.17 SOC_RESET

This is an SoC integration parameter to allow integrating HLS-generated modules into a custom user-defined SmartDesign system. The parameter specifies the name of the reset signal to connect to the HLS modules. Currently, all HLS modules use the same reset. Note that the reset polarity must be active-high.

Please refer to Soc Integration Parameters in User-defined SmartDesign for more details on how to use this Tcl parameter.

Category
HLS Constraints
Value Type
String
Default Value (Based on Icicle SoC reference design)
ARESETN
Dependencies
None
Applicable Flows
SoC Flow Only
Test Status
Actively in-use
Examples
set_parameter SOC_RESET ARESETN

3.6.2.4.18 STRENGTH_REDUCTION

Strength reduction is an optimization that converts multiply-by-constant into shifts and additions:

Info: StrengthReduction: Replacing multiply by constant (i26 33038) with 3 adders:
        - (1 << 1) + (1 << 4) + (1 << 8) + (1 << 15)
Info: StrengthReduction: Replacing multiply by constant (i26 6416) with 3 adders:
        + (1 << 4) + (1 << 8) + (1 << 11) + (1 << 12)
Info: StrengthReduction: Replacing multiply by constant (i26 28784) with 3 adders:
        - (1 << 4) + (1 << 7) - (1 << 12) + (1 << 15)
Info: StrengthReduction: Replacing multiply by constant (i26 4680) with 3 adders:
        + (1 << 3) + (1 << 6) + (1 << 9) + (1 << 12)
Info: StrengthReduction: Replacing multiply by constant (i26 33024) with 1 adder:
        + (1 << 8) + (1 << 15)

This optimization saves DSP blocks on the FPGA but can also increase LUT usage in the design.

You can tune the number of adders allowed per multiplier with the constraint: STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
1
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter STRENGTH_REDUCTION 1

3.6.2.4.19 STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER

Strength reduction is an optimization that converts multiply-by-constant into shifts and additions:

Info: StrengthReduction: Replacing multiply by constant (i26 33038) with 3 adders:
        - (1 << 1) + (1 << 4) + (1 << 8) + (1 << 15)

The STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER constraint allows you to tune the number of adders allowed per multiplier (default is 3). Strength reduction for multiply-by-constants will not be performed if this requires more adders than allowed:

i26 16828 is composed of 4 adders:
- (1 << 2) + (1 << 6) + (1 << 7) + (1 << 8) + (1 << 14)
Skipping conversion otherwise would need too many additions.

In this example, we would need 4 adders which is more than the default of 3, meaning strength reduction will not occur and SmartHLS will keep the multiplier.

Category
HLS Constraints
Value Type
Integer
Valid Values
Non-negative integer
Default Value
3
Location Where Default is Specified
examples/shls.tcl
Dependencies
STRENGTH_REDUCTION must be on
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter STRENGTH_REDUCTION_ADDERS_ALLOWED_PER_MULTIPLIER 3

3.6.2.4.20 SYNTHESIS_CLOCK_PERIOD

This constraint allows the user to override the SDC clock period constraint for synthesis, P&R, and timing analysis.

By default, when this constraint is not specified, the same CLOCK_PERIOD constraint for HLS is used for the SDC clock period constraint. However, it may be useful to give a tighter SDC clock period constraint to close timing.

The clock period is specified in nanoseconds.

Category
HLS Constraints
Value Type
Decimal or integer; represents a value in nanoseconds
Valid Values
Positive decimal or positive integer
Default Value
N/A
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter SYNTHESIS_CLOCK_PERIOD 10

3.6.2.4.21 USE_FIFO_FOR_PIPELINE_REG

In a pipeline circuit where multiple stages of the circuit are concurrently active and processing different loop iterations (or function calls), pipeline registers are used to retain and propagate a variable value from the value-producing stage to the value-use stage. The pipeline registers are essentially a chain of shift registers with additional control logic. When the chain of pipeline registers is long, it may be more resource-efficient to implement the pipeline registers as a block-RAM FIFO rather than shift registers.

When this parameter is enabled, SmartHLS will examine each chain of pipeline registers and use the implementation (FIFO or shift register) that is estimated to be more resource-efficient.

Category
HLS Constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
1
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter USE_FIFO_FOR_PIPELINE_REG 1

3.6.2.4.22 COSIM_FREE_RUNNING_DATAFLOW_TOP

The COSIM_FREE_RUNNING_DATAFLOW_TOP parameter can be useful for dataflow designs which contain conditionally-executed tasks. When the top-level module uses dataflow, this parameter will make the top-level module free-running, i.e., its start signal will be tied to 1. This parameter should not be enabled if an AXI Target interface is used.

Category
HLS Constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Alpha release
Examples
set_parameter COSIM_FREE_RUNNING_DATAFLOW_TOP 1

3.6.2.4.23 AXI_RRESP_ALWAYS_ZERO

The AXI_RRESP_ALWAYS_ZERO parameter determines how the HLS module will respond when it receives an AXI read requests to an address that is not used within its address map; essentially an address decoding error. These gaps within the addresses map occur due to address alignments in the AXI target register interface for the function arguments.

By default the module will return AXI RRESP=2'b10 (slave error) when an address decoding error is detected. It is the responsibility of the initiator of the AXI read request to process the response accordingly and the returned value (AXI RDATA) will be undefined although most likely it will be zero.

This response code can be forced to always zero by setting AXI_RRESP_ALWAYS_ZERO = 1 constraint, essentially ignoring any address decoding error. One reason to ignore this error is to perform memory monitoring or memory readout of the entire address space of a given HLS module for debugging purposes. This can be done in SoftConsole or with debuggers like gdb as can be seen in the following image using the command x/128hw 0x50000000, which means "read 128 words and print them in hex format starting at address 0x50000000", which would be the base address of the HLS module:

Important: From the CPU perspective, the SmartHLS autogenerated driver API will never generate AXI read requests that result in address decoding errors, unless the generated API and the generated RTL are out of sync.
Category
HLS Constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Alpha release
Examples
set_parameter AXI_RRESP_ALWAYS_ZERO 1

3.6.2.4.24 SYNTHESIS_FSM_ENCODING

This constraint allows users override the default finite state machine encoding chosen by the synthesis tools with the specified encoding style.

The style string value specified in this parameter will be used to generate a Synopsys synthesis attribute for each state machine register in the compiled design.

Category
HLS Constraints
Value Type
String
Valid Values
"onehot", "gray", "sequential", "safe", "original" and combination of multiple valid values separated by comma.
Default Values
"onehot"
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples

set_parameter SYNTHESIS_FSM_ENCODING "onehot,safe"

Synthesis attribute for the state machine register will be generated at the output Verilog code, as follows.

reg [`W-1:0] cur_state /* synthesis syn_encoding="onehot,safe" */;

3.6.2.4.25 SYNTHESIS_ENABLE_TMR

This constraint is used to direct synthesis tools to use triple-modular redundancy (TMR) technique in the register implementation.

When this option is enabled, Synopsys attribute /* synthesis syn_radhardlevel="tmr" */ will be applied globally to the compiled design.

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter SYNTHESIS_ENABLE_TMR 1

3.6.2.4.26 SYNTHESIS_FORCE_LOGIC_MULT

This constraint is used to force all multipliers in the compiled design to be implemented as logic, to avoid any multiplier occupies dedicated hardware DSP block resource.

When this option is enabled, Synopsys attribute /* synthesis syn_multstyle="logic" */ will be applied globally to the compiled design.

Category
HLS Constraints
Value Type
Boolean
Valid Values
0, 1
Default Value
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter SYNTHESIS_FORCE_LOGIC_MULT 1

3.6.2.4.27 ADD_SYNTHESIS_GLOBAL_ATTRIBUTE

This command allows users add any Synopsys global attribute setting to the compiled design.

Category
HLS Constraints
Value Type
String
Valid Values
Any legal Synopsys global attribute setting string in Verilog format
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples

add_synthesis_global_attribute {syn_hier="fixed"}

Attribute /* synthesis syn_hier="fixed" */ will be generated and applied globally to the compiled design.

3.6.2.4.28 MINIMIZE_MATH_BLOCKS

This constraint is used to enable optimizations targeting the reduction of math blocks usage. It mainly affects 2 optimizations: wide-multiplication split algorithm, and multiplication by constant strength reduction. By setting this constraint to 1, SmartHLS will try to minimize the number of math blocks which can increase the latency and/or the logic elements (LUTs, DFFs) usage.

Category
HLS Constraint
Value Type
Boolean
Valid Values
0, 1
Default Values
0: disabled
Location Where Default is Specified
examples/shls.tcl
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter MINIMIZE_MATH_BLOCKS 1

3.6.2.4.29 READONLY_RAM_TO_ROM

When READONLY_RAM_TO_ROM is set to 1, SmartHLS would analyze memory access patterns and generate read-only RAM as ROM (Read Only Memory). This constraint is enabled by default.

Category
HLS constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
1
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter READONLY_RAM_TO_ROM 0

3.6.2.4.30 ECC_ERROR_PROBABILITY

This constraint is used for Error Correction Code error emulation. It represents the error probability (single or double-bit errors) in software and simulation.

Category
HLS constraint
Value Type
Decimal or integer
Valid Values
Decimal or integer between 0.0 and 1.0 inclusive
Default Value
0
Dependencies
None
Applicable Flows
RTG4 and PolarFire® devices
Test Status
Actively in-use
Examples
set_parameter ECC_ERROR_PROBABILITY 1.0

3.6.2.4.31 ECC_CORRECTION_PROBABILITY

This constraint is used for Error Correction Code error emulation. It represents the probability of a single-bit error when an error is detected in software and simulation.

Category
HLS constraint
Value Type
Decimal or integer
Valid Values
Decimal or integer between 0.0 and 1.0 inclusive
Default Value
0
Dependencies
None
Applicable Flows
RTG4 and PolarFire® devices
Test Status
Actively in-use
Examples
set_parameter ECC_CORRECTION_PROBABILITY 0.5

3.6.2.4.32 ECC_WARNING_MSGS_ON

This constraint is used for Error Correction Code error emulation. It enable messages from the memory RTL model when an error is detected.

Category
HLS constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
0
Dependencies
None
Applicable Flows
RTG4 and PolarFire® devices
Test Status
Actively in-use
Examples
set_parameter ECC_WARNING_MSGS_ON 1

3.6.2.4.33 ECC_ERROR_INJECTION_ON

This constraint is used for enable the Error Simulation feature for Error Correction Code.
Important: To use ECC error injection, the ECC_ERROR_PROBABILITY and ECC_CORRECTION_PROBABILITY constraints must be removed.
Category
HLS constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
0
Dependencies
None
Applicable Flows
RTG4™
Test Status
Actively in-use
Examples
set_parameter ECC_ERROR_INJECTION_ON 1

3.6.2.4.34 ACTIVE_LOW_RESET

This constraint is used for enable active low reset for the generated RTL modules. Default is 0 (active high reset).

Category
HLS constraint
Value Type
Boolean
Valid Values
0, 1
Default Value
0
Dependencies
None
Applicable Flows
All devices and flows
Test Status
Actively in-use
Examples
set_parameter ACTIVE_LOW_RESET 1