3.6.10 PolarFire Video Kit Setup Instructions

3.6.10.1 Introduction to PolarFire Video Kit Setup Instructions

These instructions describe how to setup, compile and run an example on the PolarFireVideo Kit with the MiV_RV32 Reference Design. The instructions below assume your host computer is running Linux, but similar steps can be done on Windows.

3.6.10.2 PolarFire® Video Kit Image

This is a picture of the PolarFire Video Kit:

3.6.10.3 Board Connections

The following cables must be connected to the board for use with SmartHLS :

  • Power cable (connects to 12V Power Supply Input).
  • Mini-USB cable for serial communication to the board and embedded JTAG programmer. The same cable is used for both. Alternatively, you use the External FP6 programmer.
  • Jumper J28 must be open to use the external programmer, or closed to use the embedded programmer.

3.6.10.4 Install Host PC Applications

The following programs are required to be installed on the host PC to set up the PolarFire Video Kit:

  • SmartHLS v2024.2 or newer.
  • Libero v2024.2 or newer.
  • SoftConsole v2021.3 or later.
  • A serial communication terminal of your choosing. In this guide, we will use tio.

Users need to install SoftConsole and append the RISC-V compilation tool chain to $PATH environment variable. For example, on Linux users need to run:

export PATH=$SOFTCONSOLE_PATH/riscv-unknown-elf-gcc/bin:$PATH
And on Windows Powershell, users need to run:
$env:PATH = "$env:SOFTCONSOLE_PATH\riscv-unknown-elf-gcc\bin;$env:PATH"
Where $SOFTCONSOLE_PATH and $env::SOFTCONSOLE_PATH represent the installation path of SoftConsole.
Important: Automated SoC flow support for the PolarFire Video Kit on Linux from command line is a Beta feature available starting from SmartHLS v2025.1. Earlier versions require using the manual SoC flow.

3.6.10.5 Write, compile and run a simple test program

During the test, we will open the 3 serial terminals labeled below:

  1. UART Terminal: We will use this to see the stdout from the program.
  2. SmartHLS terminal: Linux terminal that we will use to run SmartHLS commands from the command line.
  3. OpenOCD terminal: Linux terminal that we will use to launch OpenOCD manually from the command line, provided the SmartHLS version is 2025.1 or previous.

Create a temporary directory, for example, test, and use your favorite text editor to write the following 3 files under this directory:

$> mkdir test
$> cd test

Create a simple_add.c file with the following content:

#include <stdio.h>
#include <stdint.h>
 
uint32_t hw_add(uint32_t a, uint32_t b) {
   #pragma HLS function top
   #pragma HLS interface default type(axi_target)
   return a + b;
}
 
int main() {
   uint32_t sum;
   uint32_t a = 2, b = 3;
   sum = hw_add(a, b);
 
   int error = (sum != a + b);
   printf("\n%s\n", error ? "FAIL" : "PASS");
   return error;
}

Create the Makefile with the following content:

NAME=simple_add
SRCS=$(NAME).c
LOCAL_CONFIG = -shls-config=config.tcl

Create a config.tcl file:

source $env(SHLS_ROOT_DIR)/examples/shls.tcl
set_project PolarFire MPF300 MiV_SoC

Note that we used the SHLS_ROOT_DIR environment variable, it should point to where SmartHLS is installed. On the SmartHLS Terminal type the following:

$> export SHLS_ROOT_DIR=<PATH_TO_LIBERO_SOC_2025_2>/SmartHLS/SmartHLS

Now run the SmartHLS SoC flow to:

  1. Compile the hw_add function into a Verilog module.
  2. Integrate the module into the MiV_RV32 Reference Design. See MiV_RV32 Reference Design.
  3. Run RTL synthesis.
  4. Run place and route.
  5. Check timing.
  6. Program the FPGA.
  7. Cross-compile software program.
  8. Initialize the processor memory with RISC-V binary.
  9. Run the firmware with the standard output capture via UART.

3.6.10.5.1 Automated SOC Flow (Beta Version)

Starting from version v2025.1, SmartHLS supports automated SoC flow to perform the steps mentioned in Write, compile and run a simple test program on the Linux platforms via command lines. Prior to running the associated SHLS command, the following environment variables must be configured:

  • PROGRAMMER_ID
  • SERIAL_PORT
  • OPENOCD_TOOL_PATH
    Important: Regarding OpenOCD version, the pre-released OpenOCD-0.12.0-4 from Microchip PIC64GX Curiosity Kit Support needs to be used to realize the step 8 and 9 mentioned in Write, compile and run a simple test program. Since the openocd binary is bundled in every compressed release asset, users simply need to do the following:
    • Download and extract the compressed asset.
    • Configure OPENOCD_TOOL_PATH to the bin sub-directory of the openocd directory.
The command below will invoke all these tasks as they are prerequisites to program the FPGA, cross-compile the simple_add.c program and run the generated hls_output/simple_add.elf on board:
$> shls -a soc_accel_proj_run

3.6.10.5.2 Manual SOC Flow

For versions 2024.2 or previous, SmartHLS™ only supports manual SoC flow to perform the steps mentioned in Write, compile and run a simple test program. Prior to running the associated SHLS command, PROGRAMMER_ID environment variable needs to be configured.

The command below will invoke all steps 1 to 6 (see Write, compile and run a simple test program) as they are prerequisites to program the FPGA. This will take a few minutes:
$> shls -a soc_accel_proj_program
Now, create a gdb.txt file that is used by gdb to connect to OpenOCD, load the .elf binary into the MiV_RV32’s memory and run the code:
set $target_riscv = 1
set mem inaccessible-by-default off
set arch riscv:rv32
target extended-remote localhost:3333
load
run
Cross-compile the simple_add.c program. This will generate a hls_output/simple_add.elf file.
$> shls -a soc_sw_compile_accel
In the UART terminal open the UART connection. Please note that your device may be different:
$> tio /dev/ttyUSB0 -b 115200
In the OpenOCD terminal launch OpenOCD:
$> openocd -f board/microsemi-riscv.cfg
Now go back to the SmartHLS terminal and run gdb to execute the code on the MiV_RV32.
$> riscv64-unknown-elf-gdb ./hls_output/simple_add.elf -x ./gdb.txt

At this point you should see the word PASS in the UART terminal. You can type Ctrl+C and then press q to terminate the gdb session.

Also, you can press Ctrl+C on the OpenOCD terminal to close the program, otherwise it would not release the JTAG cable.