1.5.1.1 Initialization
In the code of the MAC-RT PLC & Go example application, the G3 MAC RT driver
initialization is performed during the first states of the state machine implemented in
the function
APP_PLC_Tasks:APP_PLC_STATE_IDLEinitializes the variables related to the transmission coupling stage.APP_PLC_STATE_INITopens the G3 MAC RT driver to load the G3-PLC MAC-RT binary. If this state is reached due to a frequency band change (APP_PLC_STATE_SET_BAND), the G3 MAC RT driver needs to be initialized first. Just before opening the driver, the G3 MAC RT driver initialization callback is set. This callback will be called when G3 MAC RT is ready (G3-PLC MAC-RT binary loaded completely and validated) and it is used to configure the initial PLC PHY and MAC-RT parameters (PIBs), including:- Transmission coupling
parameters. This is always required. It can be done using the function
SRV_PCOUP_Set_Config. - The MAC header used for
transmission is initialized. PAN ID (
MAC_RT_PIB_PAN_ID) and short address (MAC_RT_PIB_SHORT_ADDRESS) are set in the G3-PLC MAC-RT. PAN ID is configured byCONF_PAN_IDand short address is chosen randomly. The destination address is broadcast by default (MAC_RT_SHORT_ADDRESS_BROADCAST). The source/destination address and the PAN ID can be configured later through the console menu. - Static notching
(
MAC_RT_PIB_TONE_MASK) only ifAPP_PLC_STATIC_NOTCHING_ENABLEis not 0. Each carrier corresponding to the frequency band can be notched (no energy is sent in those carriers). Each carrier is represented by one bit (1: carrier used; 0: carrier notched). By default it is all 1's in the PLC device (static notching disabled). The same Tone Mask must be set in both transmitter and receiver, otherwise they do not understand each other. - The PLC PHY version is read.
- Transmission coupling
parameters. This is always required. It can be done using the function
APP_PLC_STATE_OPENwaits for the G3 MAC RT driver to be ready (G3-PLC MAC-RT binary loaded completely and validated). Once the G3 MAC RT driver is ready:- The G3 MAC RT driver and
PVDD monitor service callbacks are set in order to receive different
events:
- Reception parameters event is managed by the
APP_PLC_RxParamsIndCallbackfunction to indicate the parameters of the PLC messages received. - Data indication
event is managed by the
APP_PLC_DataIndCallbackfunction to process all the PLC messages received. The parameters of the received message will be reported first inAPP_PLC_RxParamsIndCallback. - Data confirm
event is managed by the
APP_PLC_DataCfmCallbackfunction to process the results of PLC transmissions. - Exception events
are managed by the
APP_PLC_ExceptionCallbackfunction. - PLC sleep mode
disable event is managed by the
APP_PLC_SleepModeDisableCallbackfunction to restart the configuration once sleep mode is disabled. - PVDD monitor
events are managed by the
APP_PLC_PVDDMonitorCallbackfunction to enable/disable the PLC transmission.
- Reception parameters event is managed by the
- The PVDD monitor service is started, needed to enable/disable the transmission of the PL460 device using the TXEN pin. The PVDD voltage is monitored and PLC transmission is disabled in case the voltage is not in the expected range, to avoid PL460 damage. If the PVDD voltage is in the expected range, PLC transmission is enabled.
case APP_PLC_STATE_OPEN: { /* Check PLC transceiver */ if (DRV_G3_MACRT_Status(DRV_G3_MACRT_INDEX_0) == DRV_G3_MACRT_STATE_READY) { /* Configure PLC callbacks */ DRV_G3_MACRT_ExceptionCallbackRegister(appPlc.drvPlcHandle, APP_PLC_ExceptionCallback); DRV_G3_MACRT_TxCfmCallbackRegister(appPlc.drvPlcHandle, APP_PLC_DataCfmCallback); DRV_G3_MACRT_DataIndCallbackRegister(appPlc.drvPlcHandle, APP_PLC_DataIndCallback); DRV_G3_MACRT_RxParamsIndCallbackRegister(appPlc.drvPlcHandle, APP_PLC_RxParamsIndCallback); DRV_G3_MACRT_SleepIndCallbackRegister(appPlc.drvPlcHandle, APP_PLC_SleepModeDisableCallback); /* Enable PLC Transmission */ DRV_G3_MACRT_EnableTX(appPlc.drvPlcHandle, true); /* Enable PLC PVDD Monitor Service */ SRV_PVDDMON_CallbackRegister(APP_PLC_PVDDMonitorCallback, 0); SRV_PVDDMON_Start(SRV_PVDDMON_CMP_MODE_OUT); /* Init Timer to handle blinking led */ appPlc.tmr1Handle = SYS_TIME_CallbackRegisterMS(APP_PLC_Timer1_Callback, 0, LED_BLINK_RATE_MS, SYS_TIME_PERIODIC); /* Set PLC state */ appPlc.state = APP_PLC_STATE_WAITING; } } break;- The G3 MAC RT driver and
PVDD monitor service callbacks are set in order to receive different
events: