1.5.1.3 Reception
When G3 MAC-RT layer receives a PLC message, first it checks the Frame Check Sequence
(FCS, CRC), so it is not needed to check it in upper layers. If the FCS is correct, the
frame is decoded and depending on the destination PAN identifier and destination address
it is reported to the upper layer:
- If the PAN ID is different to the PAN ID
configured by the upper layer (
MAC_RT_PIB_PAN_ID) and is not the Broadcast PAN ID (0xFFFF), a communication status indication event is reported throughDRV_G3_MACRT_COMM_STATUS_IND_CALLBACK. The only parameter is a pointer to the received MAC header. This callback is not set in this example. For additional information about the usage of this event, refer to the G3-PLC specification. - If the frame type is beacon, it is always processed. Otherwise, if the
destination PAN ID is the Broadcast PAN ID or is the same as the PAN ID
configured by the upper layer, and the destination address is the Broadcast
Address (0xFFFF) or is the same as the address configured by the upper layer
(
MAC_RT_PIB_SHORT_ADDRESS,MAC_RT_PIB_MANUF_EXTENDED_ADDRESS), the frame is processed and acknowledgment (ACK) is sent if requested in the MAC header (ackRequestbit on theMAC_RT_FRAME_CONTROLstructure). If the frame is processed and it is not duplicated or repetition:- If the frame type is MAC command (Beacon Request or Tone Map Response)
it is automatically handled by MAC-RT and is not reported to the upper
layer.
- Beacon Request: Beacon frame is sent as response.
- Tone Map Response: Neighbor table is updated with modulation and Tone Map information for the transmitter node.
- If the frame type is Beacon or Data, it is reported to the upper layer
in two steps:
- Reception
parameters indication event: Specific to G3-PLC MAC
implementation. It is processed in the callback function
APP_PLC_RxParamsIndCallback. This callback receives as parameter a data structure of typeMAC_RT_RX_PARAMETERS_OBJ, containing all the available information from the message. - Reception data
indication event: Reception of standard 802.15.4 MAC data frame,
handled by callback
APP_PLC_DataIndCallbackwhere the pointer to received data (pData) and length in bytes (length) are given.
- Reception
parameters indication event: Specific to G3-PLC MAC
implementation. It is processed in the callback function
- If the frame type is MAC command (Beacon Request or Tone Map Response)
it is automatically handled by MAC-RT and is not reported to the upper
layer.
Structure MAC_RT_RX_PARAMETERS_OBJ
The reception parameters are stored in the data structure
MAC_RT_RX_PARAMETERS_OBJ, defined in
drv_g3_macrt_comm.h.// *****************************************************************************
/* G3 MAC RT Reception parameters
Summary
This struct includes information to describe any new received message.
Remarks:
None
*/
typedef struct __attribute__((packed, aligned(1))) {
/* High Priority */
bool highPriority;
/* PDU Link Quality */
uint8_t pduLinkQuality;
/* Phase Differential */
uint8_t phaseDifferential;
/* Modulation Type */
MAC_RT_MOD_TYPE modType;
/* Modulation Scheme */
MAC_RT_MOD_SCHEME modScheme;
/* Tone map */
MAC_RT_TONE_MAP toneMap;
/* Tone map Response */
MAC_RT_TONE_MAP_RSP_DATA toneMapRsp;
} MAC_RT_RX_PARAMETERS_OBJ;
Where:highPriority: Indicates if the frame was sent with high priority.pduLinkQuality: PDU Link Quality (LQI).phaseDifferential: Phase difference with transmitting node in multiples of 60 degrees (values from 0 to 5). Derived from PDC field in PHY header (FCH) and zero-crossing time. Value 6 indicates that zero-crossing time is not available.modType: Modulation type of the received frame.modTypeValue Description MAC_RT_MOD_ROBUST 0 BPSK Robust (4 repetitions) Modulation Type MAC_RT_MOD_BPSK 1 BPSK Modulation Type MAC_RT_MOD_QPSK 2 QPSK Modulation Type MAC_RT_MOD_8PSK 3 8PSK Modulation Type MAC_RT_MOD_16QAM 4 16QAM Modulation Type. Not supported. modScheme: Modulation scheme of the received frame.modSchemeValue Description MAC_RT_MOD_SCHEME_DIFFERENTIAL 0 Differential Modulation Scheme MAC_RT_MOD_SCHEME_COHERENT 1 Coherent Modulation Scheme toneMap: Tone Map (Dynamic Notching) in received frame. Each bit corresponds to a sub-band of carriers and it indicates if such carriers carry message data (1) or pseudo-random data (0)./* Tone Map size for Cenelec(A,B) bandplan */ #define TONE_MAP_SIZE_CENELEC 1 /* Tone Map size for FCC bandplan */ #define TONE_MAP_SIZE_FCC 3 /* Tone Map size for ARIB bandplan */ #define TONE_MAP_SIZE_ARIB 3 #define MAX_PHY_TONE_GROUPS 24 // ***************************************************************************** /* G3 Tone Map Summary Tone Map definition supported by G3 spec. Remarks: None */ typedef struct { uint8_t toneMap[(MAX_PHY_TONE_GROUPS + 7) / 8]; } MAC_RT_TONE_MAP;toneMapRsp: Tone Map Response data. It contains the most optimal modulation and Tone Map for the transmitter node, in terms of data-rate and robustness.// ***************************************************************************** /* G3 Tone map response data Summary This struct includes modulation type, modulation scheme and Tone Map data Remarks: For more information about Tone Map Response functionality, please refer to G3 Specification */ typedef struct { /* Modulation type */ MAC_RT_MOD_TYPE modType; /* Modulation scheme */ MAC_RT_MOD_SCHEME modScheme; /* Tone Map */ MAC_RT_TONE_MAP toneMap; } MAC_RT_TONE_MAP_RSP_DATA;