1.1.2.3 SAMD20 Xplained Pro

The following figure shows the SAMD20 Xplained Pro board connected to PL460-EK expansion board.

Figure 1-9. SAMD20 Xplained Pro + PL460-EK

PL460-EK is connected to XPRO Interface connector (EXT1) of SAMD20 Xplained Pro. A 15V DC jack must be plugged into PL460-EK in order to supply the power for PLC transmission. For additional information about PL460-EK, refer to the user guide.

PVDD Monitor functionality on this platform requires a change in resistors on PL460-EK to meet expected voltage levels at ADC input of SAMD20. For such reason, PVDD Monitor is disabled by means of APP_PLC_DISABLE_PVDDMON macro definition.
Figure 1-10. Resistors to Be Replaced on PL460-EK
The proper resistor values are already configured on MCC for provided projects.
Figure 1-11. Resistor Values Configured on MCC

SAMD20 examples are only provided with PLC support. Due to memory constraints, the Hybrid (PLC and RF) version is not provided on this platform.

The USB connector of SAMD20 Xplained Pro can be used to:
  • Send/receive USI messages to/from Microchip Hybrid Sniffer PC Tool. UART baud-rate is configured at 115200 bps (it cannot be higher due to hardware limitations on this board).
  • Flash/debug the SAMD20 device with the on-board J-link debugger

For additional information about SAMD20 Xplained Pro, refer to the user guide.