TCPIP_SNTP_TimeStampGet Function

C

TCPIP_SNTP_RESULT TCPIP_SNTP_TimeStampGet(
    TCPIP_SNTP_TIME_STAMP* pTStamp, 
    uint32_t* pLastUpdate
);

Description

This function gets the last valid timestamp obtained from a NTP server.

Preconditions

The TCP/IP Stack should have been initialized.

Parameters

ParametersDescription
pTStampPointer to a 64-bit buffer to store the last NTP timestamp. Could be NULL if the timestamp is not needed.
pLastUpdatePointer to store the last timestamp. Update tick could be NULL if the update time is not needed.

Returns

  • SNTP_RES_OK - If the call succeeded.
  • SNTP_RES_TSTAMP_STALE error code - If there is no recent timestamp.
  • SNTP_RES_TSTAMP_ERROR error code - If there is no available timestamp.

Remarks

The timestamp is returned in host order (Little Endian) with the most significant 32 bits representing seconds and the least significant 32 bits representing fraction of seconds (seconds/2^32).