TCPIP_SNTP_ConnectionParamSet Function
C
TCPIP_SNTP_RESULT TCPIP_SNTP_ConnectionParamSet(
TCPIP_NET_HANDLE netH,
IP_ADDRESS_TYPE ntpConnType,
const char* ntpServer
);
Description
This function sets the parameters for the next SNTP connections.
Preconditions
The TCP/IP Stack should have been inititialized.
Parameters
Parameters | Description |
---|---|
netH | New interface to use as default SNTP interface. If 0, the current interface is not changed. |
ntpConnType | Type of connection to make: IPv4 or IPv6. If IP_ADDRESS_TYPE_ANY, the current setting is not changed. |
ntpServer | The NTP server to be used; name or IP address can be used. If NULL or empty, SNTP won't attempt any connection. |
Returns
- SNTP_RES_OK - If the call succeeded.
- TCPIP_SNTP_RESULT error code - If the call did not succeed.
Remarks
None.