TCPIP_DHCPS_LeaseEntryGet Function
C
TCPIP_DHCPS_LEASE_HANDLE TCPIP_DHCPS_LeaseEntryGet(
TCPIP_NET_HANDLE netH,
TCPIP_DHCPS_LEASE_ENTRY* pLeaseEntry,
TCPIP_DHCPS_LEASE_HANDLE leaseHandle
);
Description
This function returns a lease entry for the TCPIP_DHCPS_LEASE_HANDLE. if the lease entry is not present for that TCPIP_DHCPS_LEASE_HANDLE, then it will return the next valid lease entry.
Preconditions
The DHCP server module must be initialized.
Parameters
Parameters | Description |
---|---|
netH | Lease entry for this interface. |
pLeaseEntry | Client lease entry details. |
leaseHandle | Lease index. |
Returns
- non-zero TCPIP_DHCPS_LEASE_HANDLE - To be used in the subsequent calls.
- 0 - If end of list or wrong interface, or DHCP server is not running on that interface.