TCPIP_DHCP_IsEnabled Function

C

bool TCPIP_DHCP_IsEnabled(
    TCPIP_NET_HANDLE hNet
);

Description

This function returns the current state of the DHCP client on the specified interface.

Preconditions

The DHCP module must be initialized.

Parameters

ParametersDescription
hNetInterface to query.

Returns

  • True - If the DHCP client service is enabled on the specified interface.
  • False - If the DHCP client service is not enabled on the specified interface.

Remarks

None.