TCPIP_DHCP_IsServerDetected Function
C
bool TCPIP_DHCP_IsServerDetected(
TCPIP_NET_HANDLE hNet
);
Description
This function determines if the DHCP client on the specified interface received any reply from a DHCP server.
Preconditions
The DHCP module must be initialized.
Parameters
Parameters | Description |
---|---|
hNet | Interface to query. |
Returns
- True - At least one DHCP server is attached to the specified network interface.
- False - No DHCP servers are currently detected on the specified network interface.
Remarks
None.