TCPIP_ARP_Probe Function

C

TCPIP_ARP_RESULT TCPIP_ARP_Probe(
    TCPIP_NET_HANDLE hNet, 
    IPV4_ADDR* IPAddr, 
    IPV4_ADDR* srcAddr, 
    TCPIP_ARP_OPERATION_TYPE opType
);

Description

This function transmits and ARP probe to determine the hardware address of a given IP address. The packet will use the type of operation and the source address specified as parameters.

Preconditions

The ARP module should have been initialized.

Parameters

ParametersDescription
hNetInterface to use.
IPAddrThe IP address to be resolved. The address must be specified in network byte order (big endian).
srcAddrThe source address to be used in the ARP packet.
opTypeOperation code to be set in the outgoing ARP packet.

Returns

  • ARP_RES_ENTRY_SOLVED - if the required entry is already solved.
  • ARP_RES_ENTRY_QUEUED - if the required entry was already queued.
  • ARP_RES_ENTRY_NEW - if the operation succeeded and a new entry was added (and queued for resolving).
  • ARP_RES_CACHE_FULL - if new entry could not be inserted, the cache was full.
  • ARP_RES_BAD_ADDRESS - bad address specified.
  • ARP_RES_NO_INTERFACE - no such interface.

Remarks

This function is a more advanced version of TCPIP_ARP_Resolve. It allows the caller to specify the operation type and the source address of the outgoing ARP packet. It also supports the ARP flags defined in TCPIP_ARP_OPERATION_TYPE.

No check is done for IPAddr to be valid.

To retrieve the ARP query result, call the TCPIP_ARP_IsResolved function.