TCPIP_ARP_CacheThresholdSet Function

C

TCPIP_ARP_RESULT TCPIP_ARP_CacheThresholdSet(
    TCPIP_NET_HANDLE hNet, 
    int purgeThres, 
    int purgeEntries
);

Description

This function sets the current value of the cache threshold for the selected interface. During the ARP operation, once the number of entries in the cache is greater than the purge threshold a number of purgeEntries (usually one) will be discarded.

Preconditions

The ARP module should have been initialized.

Parameters

ParametersDescription
hNetInterface handle to use.
purgeThresThreshold to start cache purging.
purgeEntriesNumber of entries to purge.

Returns

  • On Success - ARP_RES_OK.
  • On Failure - ARP_RES_NO_INTERFACE (if no such interface exists).

Remarks

None.