TCPIP_DNSS_EntryAdd Function

C

TCPIP_DNSS_RESULT TCPIP_DNSS_EntryAdd(
    const char* name, 
    IP_ADDRESS_TYPE type, 
    IP_MULTI_ADDRESS* pAdd, 
    uint32_t entryTimeout
);

Description

This function is used to add a IPv4 or IPv6 entry. Every time this is used to add either one IPv4 or IPv6 address with respect to the DNS hostname, there will be an expire time for a Host entry. "entryTimeout" parameter is used as the timeout value for this specific entry.

Preconditions

The DNS server must be initialized.

Parameters

ParametersDescription
nameHostname.
typeIP_ADDRESS_TYPE_IPV4 or IP_ADDRESS_TYPE_IPV6.
pAddIPv4 or IPv6 address.
entryTimeoutTime-out value for the entry.

Returns

  • TCPIP_DNSS_RES_OK - If entry remove is successful.
  • TCPIP_DNSS_RES_NO_ENTRY - If Hostname is NULL value and Invalid IP type.
  • TCPIP_DNSS_RES_MEMORY_FAIL - No Memory is present for IPv4 or IPv6 address type.
  • TCPIP_DNSS_RES_CACHE_FULL - If there is no space for the new entry.

Remarks

When the DNS server entryTimeout value is 0,it specifies that the entry is a permanent entry. user can remove this entry by using TCPIP_DNSS_CacheEntryRemove(). TTL time for this entry will be the value of TCPIP_DNSS_PERMANENT_ENTRY_TTL_TIME.