TCPIP_DNSS_IsEnabled Function
C
bool TCPIP_DNSS_IsEnabled(
TCPIP_NET_HANDLE hNet
);
Description
This function returns the current state of the DNS Server on the specified interface.
Preconditions
The DNS server must be initialized.
Parameters
Parameters | Description |
---|---|
hNet | Interface to query. |
Returns
- True - If the DNS Server is enabled on the specified interface.
- False - If the DNS Server is not enabled on the specified interface.
Remarks
None.