TCPIP_TCP_SocketNetSet Function

C

bool TCPIP_TCP_SocketNetSet(
    TCP_SOCKET hTCP, 
    TCPIP_NET_HANDLE hNet
);

Description

This function sets the network interface for an TCP socket

Preconditions

TCP socket should have been opened with TCPIP_TCP_ClientOpen()/TCPIP_TCP_ServerOpen(). hTCP - valid socket.

Parameters

ParametersDescription
hTCPThe TCP socket.
hNetInterface handle.

Returns

  • True - Indicates success.
  • False - Indicates failure.

Remarks

An invalid hNet can be passed (0) so that the current network interface selection will be cleared.