1.2.5.5.2 PIC32M MAC (ETHMAC) Configurations
ETHMAC Specific User Configurations
MAC Configuration file
MAC Default Configuration for Network Traffic:
Default configuration settings for low/medium/high network traffic
Default value: "Medium"
Symbol TCPIP_EMAC_TRAFFIC
Number of Tx Descriptors to be created:
Number of the TX descriptors to be created.
Because a TCP packet can span at most 3 buffers, the value should always be >= 4
The amount of memory needed per descriptor is not high (around 24 bytes) so when high MAC TX performance is needed make sure that this number is >= 8.
Default value: 8
Symbol TCPIP_EMAC_TX_DESCRIPTORS
Number of Rx Descriptors to be created:
Number of the RX descriptors to be created.
If not using the run time replenish mechanism (see below) it should match the number of dedicated buffers: TCPIP_EMAC_RX_DEDICATED_BUFFERS;
Otherwise it should be bigger than the sum of dedicated + non-dedicated buffers:
TCPIP_EMAC_RX_DESCRIPTORS > TCPIP_EMAC_RX_DEDICATED_BUFFERS + replenish_buffers
Default value: 8
Symbol TCPIP_EMAC_RX_DESCRIPTORS
Number of Dedicated MAC RX Buffers:
Number of MAC dedicated RX packet buffers.
These buffers are always owned by the MAC.
Note that the MAC driver allocates these buffers for storing the incoming network packets.
The bigger the storage capacity, the higher data throughput can be obtained.
Note that these packet buffers are allocated from the private TCP/IP heap that is specified by the TCPIP_STACK_DRAM_SIZE setting.
Default value: 4
Symbol TCPIP_EMAC_RX_DEDICATED_BUFFERS
Number of Non_Dedicated RX Buffers:
Number of non-dedicated buffers for the MAC initialization
Buffers allocated at the MAC driver initialization.
Default value: 0
Symbol TCPIP_EMAC_RX_INIT_BUFFERS
Minimum Threshold for the Buffer Replenish Process:
Minumum threshold for the buffer replenish process.
Whenever the number of RX scheduled buffers is <= than this threshold the MAC driver will allocate new non-dedicated buffers (meaning that they will be released to the TCP/IP heap once they are processed).
Setting this value to 0 disables the buffer replenishing process.
Default value: 1
Symbol TCPIP_EMAC_RX_LOW_THRESHOLD
Rx Buffer Allocate Count during Replenish Process:
Number of RX buffers to allocate when below threshold condition is detected.
If 0, the MAC driver will allocate (scheduled buffers - rxThres)
If !0, the MAC driver will allocate exactly TCPIP_EMAC_RX_LOW_FILL buffers
Default value: 2
Symbol TCPIP_EMAC_RX_LOW_FILL
Size of a RX Buffer. Should Be Multiple of 16:
Size of a RX packet buffer. Should be multiple of 16.
This is the size of all receive packet buffers processed by the ETHC.
The size should be enough to accommodate any network received packet.
If the packets are larger, they will have to take multiple RX buffers and the packet manipulation is less efficient.
Note: Together with TCPIP_EMAC_RX_DEDICATED_BUFFERS it has impact on TCPIP_STACK_DRAM_SIZE setting.
Default value: 1536
Symbol TCPIP_EMAC_RX_BUFF_SIZE
Ethernet RX Filters Selection:
MAC RX Filters
These filters define the packets that are accepted and rejected by the MAC driver
Adjust to your needs
The default value allows the processing of unicast, multicast and broadcast packets that have a valid CRC
Default value: none
Symbol TCPIP_EMAC_RX_FILTERS
Accept Broadcast Packets:
Allow the receiving of broadcast packets
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_BCAST_ACCEPT, TCPIP_EMAC_RX_FILTERS
Accept Multicast Packets:
Allow the receiving of multicast packets
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_MCAST_ACCEPT, TCPIP_EMAC_RX_FILTERS
Accept Unicast Packets:
Allow the receiving of unicast packets
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_UCAST_ACCEPT, TCPIP_EMAC_RX_FILTERS
Accept Not Me Unicast Packets:
Allow the receiving of not me unicast packets (promiscuous mode)
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_UCAST_OTHER_ACCEPT, TCPIP_EMAC_RX_FILTERS
Reject Runt Packets (< 64 bytes):
Reject small (runt) packets
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_RUNT_REJECT, TCPIP_EMAC_RX_FILTERS
Accept Runt Packets (< 64 bytes):
Accept small (runt) packets
Default value: false
Symbol TCPIP_EMAC_ETH_FILTER_RUNT_ACCEPT, TCPIP_EMAC_RX_FILTERS
Reject Packets with Wrong CRC:
The MAC RX should reject packets with wrong CRC
Default value: true
Symbol TCPIP_EMAC_ETH_FILTER_CRC_ERROR_REJECT, TCPIP_EMAC_RX_FILTERS
Accept Packets with Wrong CRC:
The MAC RX should Accept packets with wrong CRC
Default value: false
Symbol TCPIP_EMAC_ETH_FILTER_CRC_ERROR_ACCEPT, TCPIP_EMAC_RX_FILTERS
Use Auto Negotiation:
Use auto-negotiation to select the link speed and duplex
Default value: true
Symbol TCPIP_EMAC_ETH_OF_AUTO_NEGOTIATION
Use Full Duplex:
Use/Advertise full-duplex on the link
Default value: true
Symbol TCPIP_EMAC_ETH_OF_FULL_DUPLEX
Use Half Duplex:
Use/Advertise half-duplex on the link
Default value: true
Symbol TCPIP_EMAC_ETH_OF_HALF_DUPLEX
Use 100MBps:
Use/Advertise 100 Mbps on the link
Default value: true
Symbol TCPIP_EMAC_ETH_OF_100
Use 10MBps:
Use/Advertise 10 Mbps on the link
Default value: true
Symbol TCPIP_EMAC_ETH_OF_10
Allow Huge Packets:
Allow the transfer of huge/jumbo packets
Default value: false
Symbol TCPIP_EMAC_ETH_OF_HUGE_PKTS
Loopbacked At The MAC Level:
Enable MAC loopback
Default value: false
Symbol TCPIP_EMAC_ETH_OF_MAC_LOOPBACK
Loopbacked At The PHY Level:
Enable PHY loopback
Default value: false
Symbol TCPIP_EMAC_ETH_OF_PHY_LOOPBACK
Use Auto MDIX:
Use Auto MDIX on the link
Default value: true
Symbol TCPIP_EMAC_ETH_OF_MDIX_AUTO
Use Swapped MDIX:
Swap the MDIX wires
Default value: false
Symbol TCPIP_EMAC_ETH_OF_MDIX_SWAP
RMII Connection:
Use RMII MAC <-> PHY connection (otherwise MII)
Default value: true
Symbol TCPIP_EMAC_ETH_OF_RMII
EMAC Module ID:
The ID of the MAC module
Default value: "_ETH_BASE_ADDRESS"
Symbol TCPIP_EMAC_MODULE_ID
Enable Interrupt?:
Enable the MAC/Ethernet Controller interrupt
Default value: true
Symbol INTERRUPT_ENABLE
Maximum Frame Size - Longer Frames Will Be Discarded:
Maximum MAC supported RX/TX frame size.
The default value is 1536 (allows for VLAN tagged frames, although the VLAN tagged frames are discarded on RX).
On RX: any incoming ETH frame that is longer than this size will be discarded.
On TX: any frame that is longer than this size will be aborted by the MAC.
Normally there is no need to touch this value unless you know exactly the maximum size of the frames you want to process on your network.
Notes:
It can be used to control RX packets fragmentation (together with the TCPIP_EMAC_RX_BUFF_SIZE).
Always multiple of 16.
Default value: 1536
Symbol TCPIP_EMAC_MAX_FRAME
Link Maximum Transmission Unit - (576 - 1500):
Link Maximum Transmission Unit (MTU)
This symbol defines the largest network protocol data unit that can be transmitted over this link in a single frame.
It relates to the TCPIP_EMAC_MAX_FRAME value - see above.
The default value for an Ethernet link should be 1500.
The minimum value for an Eternet link should be 576.
If need to change this, make sure that the
TCPIP_EMAC_MAX_FRAME >= TCPIP_EMAC_LINK_MTU + 18
where the value 18 represents the Ethernet frame header:
12 bytes - destination + source address
2 bytes - frame type
4 bytes - FCS
Note: setting this value to 0, the maximum possible MTU will be used
Default value: 1500
Symbol TCPIP_EMAC_LINK_MTU
MAC Maximum Number of Supported RX Fragments:
MAC maximum number of supported RX fragments.
Based on the values of TCPIP_EMAC_MAX_FRAME and TCPIP_EMAC_RX_BUFF_SIZE an incoming frame may span multiple RX buffers (fragments).
Note that excessive fragmentation leads to performance degradation.
The default and recommended value should be 1.
Alternatively you can use the calculation of the number of fragments based on the selected RX sizes:
TCPIP_EMAC_RX_FRAGMENTS = ((TCPIP_EMAC_MAX_FRAME + (TCPIP_EMAC_RX_BUFF_SIZE -1 )) / (TCPIP_EMAC_RX_BUFF_SIZE))
Default value: 1
Symbol TCPIP_EMAC_RX_FRAGMENTS
Auto Flow Control Enable:
Enable MAC Auto Flow Control
This symbol enables/disables the auto flow control
When in full-duplex mode and the auto flow control is enabled, the MAC will send pause frames whenever the number of pending RX packets reached the full watermark.
Once this number drops to the empty watermark, a pause frame with pause value of 0 is transmitted, resuming the normal traffic
Default value: true
Symbol TCPIP_EMAC_AUTO_FLOW_CONTROL_ENABLE
Pause Time Value for the Auto Flow Control, bytes:
This represents the number of bytes to request the pause for when the auto flow control kicks in.
It is normally thought of in terms of RX packets: pauseBytes / rxBuffSize = pausePackets
Using bytes instead of packets allows better granularity
The value should be a multiple of 64 bytes
The range is : 64 bytes <= TCPIP_EMAC_FLOW_CONTROL_PAUSE_BYTES <= (4 MB - 64) bytes (0x3fffc0)
An usual value is 2 full packets. For example 2 * 1536 bytes
Used only when flow control is enabled
Default value: 3072
Symbol TCPIP_EMAC_FLOW_CONTROL_PAUSE_BYTES
The Full Water Mark, in Number of Packets:
An 8 bit value representing the full water mark, in number of packets
When the number of pending received packets reaches this threshold the auto flow control kicks in
A good rule to use for avoiding any packet overflow is to have enough receive room for at least 2 maximum packets, i.e.
fullWMMark = (rxScheduledBuffers x rxBuffSize) / TCPIP_EMAC_MAX_FRAME - (2 x TCPIP_EMAC_MAX_FRAME ) / rxBuffSize;
Always TCPIP_EMAC_FLOW_CONTROL_FULL_WMARK > TCPIP_EMAC_FLOW_CONTROL_EMPTY_WMARK
Used only when auto flow control is enabled
Adjust to your own value
Default value should use the calculation of the watermark based on the selected RX sizes and buffers:
TCPIP_EMAC_FLOW_CONTROL_FULL_WMARK = ((TCPIP_EMAC_RX_DEDICATED_BUFFERS * TCPIP_EMAC_RX_BUFF_SIZE) / TCPIP_EMAC_MAX_FRAME - (2 x TCPIP_EMAC_MAX_FRAME ) / TCPIP_EMAC_RX_BUFF_SIZE)
Default value: 2
Symbol TCPIP_EMAC_FLOW_CONTROL_FULL_WMARK
The Empty Water Mark, in Number of Packets:
An 8 bit value representing the empty water mark, in number of packets
When the auto flow control is active and the number of pending received packets falls reaching this threshold the auto flow control pause frames will stop
Always TCPIP_EMAC_FLOW_CONTROL_FULL_WMARK > TCPIP_EMAC_FLOW_CONTROL_EMPTY_WMARK
Used only when auto flow control is enabled
Default value could be 0: resume normal traffic when there is no pending RX packet
Default value: 0
Symbol TCPIP_EMAC_FLOW_CONTROL_EMPTY_WMARK
External PHY Device:
The external PHY connected to the MAC device
Default value: ""
Symbol DRV_INTMAC_PHY_TYPE
ETHMAC Heap Size (bytes):
Estimation of the heap size taken by the MAC driver
Default value: none
Symbol DRV_ETHMAC_HEAP_SIZE