IPV4_FRAGMENT_INFO Union

C

typedef union {
uint16_t val;
struct {
    uint16_t fragOffset : 13;
    uint16_t MF : 1;
    uint16_t DF : 1;
    uint16_t reserved : 1;
}
} IPV4_FRAGMENT_INFO;

Description

IPv4 packet fragment definition.

This is the structure of an IPv4 fragment info in the IPv4 header.

Parameters

ParametersDescription
uint16_t fragOffset : 13;Fragment offset.
uint16_t MF : 1;More fragments.
uint16_t DF : 1;Don't fragment.

Returns

None.

Remarks

None.