TCPIP_ICMPV6_CallbackRegister Function
C
ICMPV6_HANDLE TCPIP_ICMPV6_CallbackRegister(void (*callback)(TCPIP_NET_HANDLE hNetIf, uint8_t type, const IPV6_ADDR * localIP, const IPV6_ADDR * remoteIP, void * header));
Returns
ICMPV6_HANDLE
Success - Returns a valid handle
Failure - Null handle
Description
This function registers an upper-layer function to handle ICMPv6 messages that may require action at the application layer (Echo Replies, Error messages)
Remarks
None.
Preconditions
IPv6 and ICMPv6 are initialized.
Parameters
Parameters | Description |
---|---|
type | ICMPv6 header type |
localIP | IPv6 destination address of the incoming message |
remoteIP | IPv6 address of the node that originated the incoming message |
header | Pointer to the ICMPv6 header |