TCPIP_UDP_PacketHandlerRegister Function
C
TCPIP_UDP_PROCESS_HANDLE TCPIP_UDP_PacketHandlerRegister(TCPIP_UDP_PACKET_HANDLER pktHandler, const void* handlerParam);
Returns
a valid TCPIP_UDP_PROCESS_HANDLE - if the operation succeeded
NULL - if the operation failed
Description
This function registers a new packet processing handler. The caller can use the handler to be notified of incoming packets and given a chance to examine/process them.
Remarks
Currently only one packet handler is supported for the UDP module. The call will fail if a handler is already registered. Use TCPIP_UDP_PacketHandlerDeregister first Exists only if TCPIP_UDP_EXTERN_PACKET_PROCESS is true
Preconditions
UDP properly initialized
Example
TCPIP_UDP_PROCESS_HANDLE pktHandle = TCPIP_UDP_PacketHandlerRegister( myPktHandler, myParam );
Parameters
Parameters | Description |
---|---|
pktHandler | the packet handler which will be called for an incoming packet |
handlerParam | packet handler parameter |