1.2.4 Illustration
(Ask a Question)The following figure shows the design used for receiver performance of the IBIS-AMI model. The Tx is connected to the Rx through . The output of the backplane is looped back the PolarFire Evaluation kit Rx SMAs. The following figure shows the hardware setup.
The following figure shows an equivalent IBIS-AMI simulation setup.
The following section discusses the different modes.