22.3 PWM Period
The PWM period is specified by the TxPR register The PWM period can be calculated using the formula of 22.3 PWM Period. It is required to have FOSC/4 as the selected clock input to the timer for correct PWM operation.
When T2TMR is equal to T2PR, the following three events occur on the next increment cycle:
- T2TMR is cleared
- The PWM output is active. (Exception: When the PWM duty cycle = 0%, the PWM output will remain inactive.)
- The PWMxDCH and PWMxDCL register values are latched into the buffers.
Important: The Timer2 postscaler has no effect on the PWM operation.