36.1 Standard Instruction Set
The standard PIC18 instruction set adds many enhancements to the previous PIC® MCU instruction sets, while maintaining an easy migration from these PIC® MCU instruction sets. Most instructions are a single program memory word (16 bits), but there are four instructions that require two program memory locations.
Each single-word instruction is a 16-bit word divided into an opcode, which specifies the instruction type and one or more operands, which further specify the operation of the instruction.
The instruction set is highly orthogonal and is grouped into four basic categories:
- Byte-oriented operations
- Bit-oriented operations
- Literal operations
- Control operations
The PIC18 instruction set summary in Table 36-2 lists byte-oriented, bit-oriented, literal and control operations. Table 36-1 shows the opcode field descriptions.
Most byte-oriented instructions have three operands:
- The file register (specified by ‘f’)
- The destination of the result (specified by ‘d’)
- The accessed memory (specified by ‘a’)
The file register designator ‘f’ specifies which file register is to be used by the instruction. The destination designator ‘d’ specifies where the result of the operation is to be placed. If ‘d’ is zero, the result is placed in the WREG register. If ‘d’ is one, the result is placed in the file register specified in the instruction.
All bit-oriented instructions have three operands:
- The file register (specified by ‘f’)
- The bit in the file register (specified by ‘b’)
- The accessed memory (specified by ‘a’)
The bit field designator ‘b’ selects the number of the bit affected by the operation, while the file register designator ‘f’ represents the number of the file in which the bit is located.
The literal instructions may use some of the following operands:
- A literal value to be loaded into a file register (specified by ‘k’)
- The desired FSR register to load the literal value into (specified by ‘f’)
- No operand required (specified by ‘—’)
The control instructions may use some of the following operands:
- A program memory address (specified by ‘n’)
- The mode of the CALL or RETURN instructions (specified by ‘s’)
- The mode of the table read and table write instructions (specified by ‘m’)
- No operand required (specified by ‘—’)
All instructions are a single word, except for four double-word instructions. These instructions were made double-word to contain the required information in 32 bits. In the second word, the four MSbs are ‘1’s. If this second word is executed as an instruction (by itself), it will execute as a NOP
.
All single-word instructions are executed in a single instruction
cycle, unless a conditional test is true or the Program Counter is changed as a result of
the instruction. In these cases, the execution takes two instruction cycles, with the
additional instruction cycle(s) executed as a NOP
.
The double-word instructions execute in two instruction cycles.
One instruction cycle consists of four oscillator periods. Thus, for an oscillator frequency of 4 MHz, the normal instruction execution time is 1 μs. If a conditional test is true, or the Program Counter is changed as a result of an instruction, the instruction execution time is 2 μs. Two-word branch instructions (if true) would take 3 μs.
Figure 36-1 shows the general formats that the instructions can have. All examples use the convention ‘nnh’ to represent a hexadecimal number.
The Instruction Set Summary, shown in Table 36-2, lists the standard instructions recognized by the Microchip Assembler (MPASMTM).
36.1.1 Standard Instruction Set provides a description of each instruction.
Field | Description |
---|---|
|
RAM access bit a = 0: RAM location in Access RAM (BSR register is ignored) a = 1: RAM bank is specified by BSR register |
|
Bit address within an 8-bit file register (0 to 7). |
|
Bank Select Register. Used to select the current RAM bank. |
|
ALU Status bits: Carry, Digit Carry, Zero, Overflow, Negative. |
|
Destination select bit d = 0: store result in WREG d = 1: store result in file register f |
dest | Destination: either the WREG register or the specified register file location. |
|
8-bit Register file address (00h to FFh) or 2-bit FSR designator (0h to 3h). |
|
12-bit Register file address (000h to FFFh). This is the source address. |
|
12-bit Register file address (000h to FFFh). This is the destination address. |
|
Global Interrupt Enable bit. |
|
Literal field, constant data or label (may be either an 8-bit, 12-bit or a 20-bit value). |
|
Label name. |
|
The mode of the TBLPTR register for the table read and table write instructions. Only used with table read and table write instructions: |
* | No change to register (such as TBLPTR with table reads and writes) |
*+ | Post-Increment register (such as TBLPTR with table reads and writes) |
*- | Post-Decrement register (such as TBLPTR with table reads and writes) |
+* | Pre-Increment register (such as TBLPTR with table reads and writes) |
|
The relative address (2’s complement number) for relative branch instructions or the direct address for CALL/BRANCH and RETURN instructions. |
|
Program Counter. |
|
Program Counter Low Byte. |
|
Program Counter High Byte. |
|
Program Counter High Byte Latch. |
|
Program Counter Upper Byte Latch. |
|
Power-down bit. |
|
Product of Multiply High Byte. |
|
Product of Multiply Low Byte. |
|
Fast Call/Return mode select bit s = 0: do not update into/from shadow registers s = 1: certain registers loaded into/from shadow registers (Fast mode) |
|
21-bit Table Pointer (points to a Program Memory location). |
|
8-bit Table Latch. |
|
Time-out bit. |
|
Top-of-Stack. |
|
Unused or unchanged. |
|
Watchdog Timer. |
|
Working register (accumulator). |
|
Don’t care (‘0’ or ‘1’). The assembler will generate code with x = 0. It is the recommended form of use for compatibility with all Microchip software tools. |
|
7-bit offset value for Indirect Addressing of register files (source). |
|
7-bit offset value for Indirect Addressing of register files (destination). |
{ } | Optional argument. |
[text] | Indicates an indexed address. |
|
The contents of text. |
|
Specifies bit n of the register indicated by the pointer expr. |
→ | Assigned to. |
|
Register bit field. |
∈ | In the set of. |
italics | User defined term (font is Courier). |
Mnemonic, Operands |
Description | Cycles | 16-Bit Instruction Word | Status Affected |
Notes | ||||
---|---|---|---|---|---|---|---|---|---|
MSb | LSb | ||||||||
BYTE-ORIENTED OPERATIONS | |||||||||
ADDWF | f, d, a | Add WREG and f | 1 |
|
|
|
|
C, DC, Z, OV, N | 1, 2 |
ADDWFC | f, d, a | Add WREG and CARRY bit to f | 1 |
|
|
|
|
C, DC, Z, OV, N | 1, 2 |
ANDWF | f, d, a | AND WREG with f | 1 |
|
|
|
|
Z, N | 1, 2 |
CLRF | f, a | Clear f | 1 |
|
|
|
|
Z | 2 |
COMF | f, d, a | Complement f | 1 |
|
|
|
|
Z, N | 1, 2 |
CPFSEQ | f, a | Compare f with WREG, skip = | 1 (2 or 3) |
|
|
|
|
None | 4 |
CPFSGT | f, a | Compare f with WREG, skip > | 1 (2 or 3) |
|
|
|
|
None | 4 |
CPFSLT | f, a | Compare f with WREG, skip < | 1 (2 or 3) |
|
|
|
|
None | 1, 2 |
DECF | f, d, a | Decrement f | 1 |
|
|
|
|
C, DC, Z, OV, N | 1, 2, 3, 4 |
DECFSZ | f, d, a | Decrement f, Skip if 0 | 1 (2 or 3) |
|
|
|
|
None | 1, 2, 3, 4 |
DCFSNZ | f, d, a | Decrement f, Skip if Not 0 | 1 (2 or 3) |
|
|
|
|
None | 1, 2 |
INCF | f, d, a | Increment f | 1 |
|
|
|
|
C, DC, Z, OV, N | 1, 2, 3, 4 |
INCFSZ | f, d, a | Increment f, Skip if 0 | 1 (2 or 3) |
|
|
|
|
None | 4 |
INFSNZ | f, d, a | Increment f, Skip if Not 0 | 1 (2 or 3) |
|
|
|
|
None | 1, 2 |
IORWF | f, d, a | Inclusive OR WREG with f | 1 |
|
|
|
|
Z, N | 1, 2 |
MOVF | f, d, a | Move f | 1 |
|
|
|
|
Z, N | 1 |
MOVFF | fs, fd | Move fs (source) to 1st word | 2 |
|
|
|
|
None | |
fd (destination) 2nd word |
|
|
|
|
|||||
MOVWF | f, a | Move WREG to f | 1 |
|
|
|
|
None | |
MULWF | f, a | Multiply WREG with f | 1 |
|
|
|
|
None | 1, 2 |
NEGF | f, a | Negate f | 1 |
|
|
|
|
C, DC, Z, OV, N | |
RLCF | f, d, a | Rotate Left f through Carry | 1 |
|
|
|
|
C, Z, N | 1, 2 |
RLNCF | f, d, a | Rotate Left f (No Carry) | 1 |
|
|
|
|
Z, N | |
RRCF | f, d, a | Rotate Right f through Carry | 1 |
|
|
|
|
C, Z, N | |
RRNCF | f, d, a | Rotate Right f (No Carry) | 1 |
|
|
|
|
Z, N | |
SETF | f, a | Set f | 1 |
|
|
|
|
None | 1, 2 |
SUBFWB | f, d, a | Subtract f from WREG with borrow | 1 |
|
|
|
|
C, DC, Z, OV, N | |
SUBWF | f, d, a | Subtract WREG from f | 1 |
|
|
|
|
C, DC, Z, OV, N | 1, 2 |
SUBWFB | f, d, a | Subtract WREG from f with borrow | 1 |
|
|
|
|
C, DC, Z, OV, N | |
SWAPF | f, d, a | Swap nibbles in f | 1 |
|
|
|
|
None | 4 |
TSTFSZ | f, a | Test f, skip if 0 | 1 (2 or 3) |
|
|
|
|
None | 1, 2 |
XORWF |
f, d, a |
Exclusive OR WREG with f |
1 |
|
|
|
|
Z, N |
|
BIT-ORIENTED OPERATIONS | |||||||||
BCF | f, b, a | Bit Clear f | 1 |
|
|
|
|
None | 1, 2 |
BSF | f, b, a | Bit Set f | 1 |
|
|
|
|
None | 1, 2 |
BTFSC | f, b, a | Bit Test f, Skip if Clear | 1 (2 or 3) |
|
|
|
|
None | 3, 4 |
BTFSS | f, b, a | Bit Test f, Skip if Set | 1 (2 or 3) |
|
|
|
|
None | 3, 4 |
BTG |
f, b, a |
Bit Toggle f |
1 |
|
|
|
|
None |
1, 2 |
CONTROL OPERATIONS | |||||||||
BC | n | Branch if Carry | 1 (2) |
|
|
|
|
None |
4 |
BN | n | Branch if Negative | 1 (2) |
|
|
|
|
None |
|
BNC | n | Branch if Not Carry | 1 (2) |
|
|
|
|
None |
|
BNN | n | Branch if Not Negative | 1 (2) |
|
|
|
|
None |
|
BNOV | n | Branch if Not Overflow | 1 (2) |
|
|
|
|
None |
|
BNZ | n | Branch if Not Zero | 1 (2) |
|
|
|
|
None |
|
BOV | n | Branch if Overflow | 1 (2) |
|
|
|
|
None |
|
BRA | n | Branch Unconditionally | 2 |
|
|
|
|
None |
|
BZ | n | Branch if Zero | 1 (2) |
|
|
|
|
None |
|
CALL | k, s | Call subroutine 1st word |
2 |
|
|
|
|
None |
|
2nd word |
|
|
|
|
|||||
CLRWDT |
— |
Clear Watchdog Timer | 1 |
|
|
|
|
TO, PD | |
DAW | — | Decimal Adjust WREG | 1 |
|
|
|
|
C | |
GOTO | k |
Go to address 1st word
|
2 |
|
|
|
|
None | |
2nd word |
|
|
|
|
|||||
NOP | — | No Operation | 1 |
|
|
|
|
None | |
NOP | — | No Operation | 1 |
|
|
|
|
None | |
POP |
— |
Pop top of return stack (TOS) | 1 |
|
|
|
|
None | |
PUSH | — | Push top of return stack (TOS) | 1 |
|
|
|
|
None | |
RCALL | n | Relative Call | 2 |
|
|
|
|
None | |
RESET | Software device Reset | 1 |
|
|
|
|
All | ||
RETFIE | s | Return from interrupt enable | 2 |
|
|
|
|
GIE/GIEH, PEIE/GIEL |
|
RETLW | k | Return with literal in WREG | 2 |
|
|
|
|
None | |
RETURN | s | Return from Subroutine | 2 |
|
|
|
|
None | |
SLEEP |
— |
Go into Standby mode |
1 |
|
|
|
|
TO, PD |
|
LITERAL OPERATIONS | |||||||||
ADDLW | k | Add literal and WREG | 1 |
|
|
|
|
C, DC, Z, OV, N | |
ANDLW | k | AND literal with WREG | 1 |
|
|
|
|
Z, N | |
IORLW | k | Inclusive OR literal with WREG | 1 |
|
|
|
|
Z, N | |
LFSR | f, k | Move literal (12-bit) 2nd word | 2 |
|
|
|
|
None | |
to FSR(f) 1st word |
|
|
|
|
|||||
MOVLB | k | Move literal to BSR<3:0> | 1 |
|
|
|
|
None | |
MOVLW | k | Move literal to WREG | 1 |
|
|
|
|
None | |
MULLW | k | Multiply literal with WREG | 1 |
|
|
|
|
None | |
RETLW | k | Return with literal in WREG | 2 |
|
|
|
|
None | |
SUBLW | k | Subtract WREG from literal | 1 |
|
|
|
|
C, DC, Z, OV, N | |
XORLW |
k |
Exclusive OR literal with WREG |
1 |
|
|
|
|
Z, N |
|
DATA MEMORY ↔ PROGRAM MEMORY OPERATIONS | |||||||||
TBLRD* | Table Read | 2 |
|
|
|
|
None | ||
TBLRD*+ | Table Read with post-increment |
|
|
|
|
None | |||
TBLRD*- | Table Read with post-decrement |
|
|
|
|
None | |||
TBLRD+* | Table Read with pre-increment |
|
|
|
|
None | |||
TBLWT* | Table Write | 2 |
|
|
|
|
None | ||
TBLWT*+ | Table Write with post-increment |
|
|
|
|
None | |||
TBLWT*- | Table Write with post-decrement |
|
|
|
|
None | |||
TBLWT+* |
Table Write with pre-increment |
|
|
|
|
None |
- When a PORT register is modified as a function of itself (e.g., MOVF PORTB, 1, 0), the value used will be that value present on the pins themselves. For example, if the data latch is ‘1’ for a pin configured as input and is driven low by an external device, the data will be written back with a ‘0’.
- If this instruction is executed on the TMR0 register (and where applicable, ‘d’ = 1), the prescaler will be cleared if assigned.
- If Program Counter (PC) is modified
or a conditional test is true, the instruction requires two cycles. The second cycle
is executed as a
NOP
. - Some instructions are two-word
instructions. The second word of these instructions will be executed as a
NOP
unless the first word of the instruction retrieves the information embedded in these 16 bits. This ensures that all program memory locations have a valid instruction.