11.1.4.2 PFM Word Write Sequence
The sequence of events for programming an erased single word of internal program memory location should be:
- Set NVMADR with the target word address.
- Load NVMDAT with desired word.
- Disable interrupts.
- Execute the word/byte write unlock sequence (see 11.1.2 NVM Unlock Sequence).
- WR bit is set as last step in the unlock sequence.
- The CPU will stall for the duration of the write (about 50 μs using internal timer).
- Re-enable interrupts.
- Verify the memory (word read).
Writing a Word of Program Flash Memory
; Code sequence to program one erased word of PFM
; Target address is in WORD_ADDR_UPPER:WORD_ADDR_HIGH:WORD_ADDR_LOW
; Target data is in WORD_HIGH_BYTE:WORD_LOW_BYTE
; Calling routine should check WREG for the following errors:
;
; 00h = Successful modification
; 03h = Write error
;
WORD_WRITE:
MOVF WORD_ADDR_UPPER, W ; load NVMADR with the target
MOVWF NVMADRU ; address of the word
MOVF WORD_ADDR_HIGH, W
MOVWF NVMADRH
MOVF WORD_ADDR_LOW, W
MOVWF NVMADRL
MOVF WORD_HIGH_BYTE, W ; load NVMDAT with desired
MOVWF NVMDATH ; word
MOVF WORD_LOW_BYTE, W
MOVWF NVMDATL
BCF INTCON, GIE ; disable interrupts
BSF NVMCON0, NVMEN ; enable NVM
PROGRAM_WORD:
; ----- Required Sequence -----
MOVLW 055h
MOVWF NVMCON2 ; first unlock byte = 055h
MOVLW 0AAh
MOVWF NVMCON2 ; second unlock byte = 0AAh
BSF NVMCON1, WR ; start word programming (CPU stall)
; ------------------------------
BTFSC NVMCON0, NVMERR ; Verify no error occurred during write
BRA NVM_WRERR ; return sector write error code
VERIFY_WORD:
BSF NVMCON0, RD ; Retrieve word from PFM
MOVF WORD_HIGH_BYTE, W ; Verify high byte
CPFSEQ NVMDATH
BRA NVM_RDERR ; not equal - return error code
MOVF WORD_LOW_BYTE, W ; Verify low byte
CPFSEQ NVMDATL
BRA NVM_RDERR ; not equal - return error code
CLRF WREG,F ; return with no error
BRA NVM_EXIT
NVM_RDERR:
MOVLW 01h
BRA NVM_EXIT
NVM_WRERR:
MOVLW 03h
NVM_EXIT:
BCF NVMCON0, NVMEN ; disable NVM
BSF INTCON, GIE ; re-enable interrupts
RETURN