9.4 Watchdog Window
The Windowed Watchdog Timer has an optional Windowed mode that is
controlled by the WDTCWS Configuration bits and WINDOW bits. In the Windowed mode, the CLRWDT
instruction must occur within the allowed window of the WDT period. Any
CLRWDT
instruction that occurs outside of this
window will trigger a window violation and will cause a WWDT Reset, similar to a WWDT
time-out. See Figure 9-2 for an example.
The window size is controlled by the WINDOW Configuration bits, or
the WINDOW bits, if WDTCWS = 111
.
The five Most Significant bits of the WDTTMR register are used to determine whether the window is open, as defined by the WINDOW bits.
In the event of a window violation, a Reset will be generated and the WDTWV bit of the PCON0 register will be cleared. This bit is set by a POR or can be set in firmware.